Inconsistency of ADC Conversion value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Inconsistency of ADC Conversion value

2,392 Views
gauravbanyal
Contributor IV

Hello,

I am using MKL03Z32VFG4 and using the ADC0 peripheral for measuring voltage.

I am using the internal voltage reference. I have seen that when I have under 1.0 volts on the analog pin, I have a certain value the ADC returns. Then if I increase to 1.1volts, the value is smaller than at 1.0 volts. And subsequently, as I go on increasing voltage on the analog pin, the values that the ADC returns are incrementing / decrementing together with the increment/decrement of the voltage. 

Please let me know how can I get rid of that value going low even though the voltage level on the pin is higher.

My code is as follows:

================================

#define BATT_ADC16_BASE ADC0
#define BATT_ADC16_CHANNEL_GROUP 0U
#define BATT_ADC16_USER_CHANNEL 15U /* PTA0, ADC0_SE15 */

#define BATT_ADC16_IRQn ADC0_IRQn

#define BATT_VOLTAGE_READING_AVAILABLE ADC0_IRQHandler

void batt_mon_init(){

EnableIRQ(BATT_ADC16_IRQn);
ADC16_GetDefaultConfig(&adc16ConfigStruct);
adc16ConfigStruct.clockDivider = kADC16_ClockDivider1;
adc16ConfigStruct.referenceVoltageSource = kADC16_ReferenceVoltageSourceValt;
adc16ConfigStruct.enableHighSpeed = true;
ADC16_Init(BATT_ADC16_BASE, &adc16ConfigStruct);
ADC16_EnableHardwareTrigger(BATT_ADC16_BASE, false); /* Make sure the software trigger is used. */
#if defined(FSL_FEATURE_ADC16_HAS_CALIBRATION) && FSL_FEATURE_ADC16_HAS_CALIBRATION
if (kStatus_Success != ADC16_DoAutoCalibration(BATT_ADC16_BASE))
{
LOG_E("ADC16_DoAutoCalibration() Failed.\r\n");
}
#endif /* FSL_FEATURE_ADC16_HAS_CALIBRATION */

adc16ChannelConfigStruct.channelNumber = BATT_ADC16_USER_CHANNEL;
adc16ChannelConfigStruct.enableInterruptOnConversionCompleted = true; /* Enable the interrupt. */
#if defined(FSL_FEATURE_ADC16_HAS_DIFF_MODE) && FSL_FEATURE_ADC16_HAS_DIFF_MODE
adc16ChannelConfigStruct.enableDifferentialConversion = false;
#endif /* FSL_FEATURE_ADC16_HAS_DIFF_MODE */
}

void read_battery_level(){

g_Adc16ConversionDoneFlag = false;
/*
When in software trigger mode, each conversion would be launched once calling the "ADC16_ChannelConfigure()"
function, which works like writing a conversion command and executing it. For another channel's conversion,
just to change the "channelNumber" field in channel configuration structure, and call the function
"ADC16_ChannelConfigure()"" again.
Also, the "enableInterruptOnConversionCompleted" inside the channel configuration structure is a parameter for
the conversion command. It takes affect just for the current conversion. If the interrupt is still required
for the following conversion, it is necessary to assert the "enableInterruptOnConversionCompleted" every time
for each command.
*/
ADC16_SetChannelConfig(BATT_ADC16_BASE, BATT_ADC16_CHANNEL_GROUP, &adc16ChannelConfigStruct);
}

void BATT_VOLTAGE_READING_AVAILABLE(void)
{
g_Adc16ConversionDoneFlag = true;
static volatile uint32_t avgAdc16ConvValue = 0;
static volatile int i=0;
/* Read conversion result to clear the conversion completed flag. */
volatile uint32_t adc16ConversionValue = ADC16_GetChannelConversionValue(BATT_ADC16_BASE, BATT_ADC16_CHANNEL_GROUP);

if(i<200){
if (i==0) avgAdc16ConvValue = adc16ConversionValue;
uint32_t quotient = (avgAdc16ConvValue+adc16ConversionValue)/2;
uint32_t remainder = (avgAdc16ConvValue+adc16ConversionValue)%2;
avgAdc16ConvValue = quotient+remainder;
}
i++;

if (i == 200){
i=0;
(void) enqueueEvent( mainEventQueue, ADC_MEASUREMENT_AVAILABLE, (invisible_event_params_t) { .uIntVal = avgAdc16ConvValue }, event_batt_measurement_available );
}
else{
read_battery_level();
}
}

=====================

Best regards,

Gaurav.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,189 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Gaurav,

The ADC can be configured to accept one of the two voltage reference pairs as the reference voltage (VREFSH and VREFSL) used for conversions. The two pairs are external (VREFH and VREFL) and alternate (VALTH and VALTL).

So I think your internal reference means VALTH and VALTL.

In KL03 VREF_OUT connected as the VALT reference. You can find the descriptions in page 381 in the reference manual.

Regards

Jing

0 Kudos
Reply

2,189 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Gaurav,

Have you connect a capacitor to the ground on VREF_OUT pin?

Regards

Jing

0 Kudos
Reply

2,189 Views
gauravbanyal
Contributor IV

Hi,

I am using the internal reference voltage for the ADC. So I understand I cannot connect the capacitor to any pin on the microcontroller as you have suggested?

best regards,

Gaurav

0 Kudos
Reply