Implementing a 50Hz PLL for on-grid inverter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing a 50Hz PLL for on-grid inverter

2,282 Views
arunkumar1989
Contributor I

Hello Everyone,

Are there any examples on implementing a 50Hz digital PLL using the Kenetis K60 MCU?

If there are any ready made ICs avalable from NXP it would be really helpfull.

Thanks,

Arun

Labels (1)
0 Kudos
Reply
1 Reply

2,044 Views
bobpaddock
Senior Contributor III

I'm guessing you are looking to clean up the incoming zero crossing signal to synchronize with the line?


Synchronized Oscillator as shown in Figure-11 will make things a lot easier by starting with a clean signal.

http://cds.linear.com/docs/en/application-note/an12fa.pdf 

Feed the signal into one of the Input Capture timer pins.

If dealing with three-phase will need two zero crossing detectors to determine phase rotation automatically.

This can also help as at some phase angles the transistors/SCRs will be firing at the zero crossing point on one of the phases.

Software Phase Locked Loop | Hackaday.io may be of some interest as well.

More on Synchronized Oscillators here:

My favorite Application Notes and Old Obscure Data Sheets 

0 Kudos
Reply