Implementing a 50Hz PLL for on-grid inverter

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Implementing a 50Hz PLL for on-grid inverter

2,400 次查看
arunkumar1989
Contributor I

Hello Everyone,

Are there any examples on implementing a 50Hz digital PLL using the Kenetis K60 MCU?

If there are any ready made ICs avalable from NXP it would be really helpfull.

Thanks,

Arun

标签 (1)
0 项奖励
回复
1 回复

2,162 次查看
bobpaddock
Senior Contributor III

I'm guessing you are looking to clean up the incoming zero crossing signal to synchronize with the line?


Synchronized Oscillator as shown in Figure-11 will make things a lot easier by starting with a clean signal.

http://cds.linear.com/docs/en/application-note/an12fa.pdf 

Feed the signal into one of the Input Capture timer pins.

If dealing with three-phase will need two zero crossing detectors to determine phase rotation automatically.

This can also help as at some phase angles the transistors/SCRs will be firing at the zero crossing point on one of the phases.

Software Phase Locked Loop | Hackaday.io may be of some interest as well.

More on Synchronized Oscillators here:

My favorite Application Notes and Old Obscure Data Sheets 

0 项奖励
回复