If I'm using a mk66 part how do I wire it for only using one usb port?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

If I'm using a mk66 part how do I wire it for only using one usb port?

ソリューションへジャンプ
1,557件の閲覧回数
jeromeronne
Contributor I

The data sheet only mentions not using both ports:

pastedImage_0.png

I'm thinking tie Vreg_IN0 to Vreg_IN1

I would use the USB1 port so I have bus detect. then float USB0_DP and USB0_DM

Vreg_out would have some caps for filtering but otherwise would not be used.

ラベル(3)
0 件の賞賛
返信
1 解決策
1,372件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

There is a Note at K66 chapter 53 USB Voltage Regulator:

When USB is not used in the application, it is recommended to connect VREGOUT and VREG_INx together and tie to ground

through a 10kΩ resistor. Do not tie directly to ground, as this causes a latch-up risk. For systems where only one of the VREG_INx pins is ever used, it is also recommended to connect the two VREG_INx pins together.

Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,373件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

There is a Note at K66 chapter 53 USB Voltage Regulator:

When USB is not used in the application, it is recommended to connect VREGOUT and VREG_INx together and tie to ground

through a 10kΩ resistor. Do not tie directly to ground, as this causes a latch-up risk. For systems where only one of the VREG_INx pins is ever used, it is also recommended to connect the two VREG_INx pins together.

Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,372件の閲覧回数
jeromeronne
Contributor I

I had decided to just tie the two regulator inputs together. It is always good to get verification that design choices are correct!

0 件の賞賛
返信