ISR in Kinetis L

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
5,384件の閲覧回数
vivacious
Contributor II

Hi,

I am looking to write an ISR in C (bare metal) for one Kinetis L.
However I didn't get any procedure to setup any particular ISR.

Can somebody guide me where should I look for these details?

.....Still better if I can get an example code.

ラベル(2)
タグ(3)
1 解決策
4,388件の閲覧回数
vivacious
Contributor II

ok...thank you one and all.

I've tested this and this works.

Well I think basic idea is that correspoinding to a IRQ function in Kinetis_sysinit.c, you have to create a function by the same name (Example UART0_IRQHandler() for UART0). The newly defined function would be the ISR for the interrut(UART0 in this case).

Let me know if I've missed anything.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,388件の閲覧回数
JimDon
Senior Contributor III

Put this in main.c:

/*

*  SET_NMI_INTERRUPT() - This will cause an NMI interrupt.

*  It is a one shot, and does not need to be reset.

*/

#define SET_NMI_INTERRUPT() SCB_ICSR |= SCB_ICSR_NMIPENDSET_MASK

volatile int nmi_counter=0;

void NMI_Handler() // override the weak definition

{

  ++nmi_counter; // Put a break point here.

}

int main(int argc,char **argv)

{ 

     while(1)

       SET_NMI_INTERRUPT();

}

|

4,389件の閲覧回数
vivacious
Contributor II

ok...thank you one and all.

I've tested this and this works.

Well I think basic idea is that correspoinding to a IRQ function in Kinetis_sysinit.c, you have to create a function by the same name (Example UART0_IRQHandler() for UART0). The newly defined function would be the ISR for the interrut(UART0 in this case).

Let me know if I've missed anything.

0 件の賞賛
返信
4,388件の閲覧回数
JimDon
Senior Contributor III

Look in kinetis_sysinit.c.

For example, if I define " void SysTick_Handler(){}" else where, that will go in the vector table due to the weak keyword.

In ARM, a plain"C" function can be an interrupt handler, as the hardware knows that when a function returns it was from an interrupt, and how to handle it.

0 件の賞賛
返信
4,388件の閲覧回数
vivacious
Contributor II

Thanks for your response Marco....though I should have mentioned that I am using CodeWarrior10.3.......

But I think this should help.......Let me check.

Looking forward to more explanations/responses ......like more generic ones.

0 件の賞賛
返信
4,388件の閲覧回数
marcopalestro
Contributor II

Hi Vivek,

I can tell you how I got working ISR for Kinetis, but I guess it depends on the toolchain you're using.

With IAR Embedded Workbench, I just declare the ISR like a normal routine:

void lptmr_isr(void)

{

    lp_seconds++;

    LPTMR0_CSR |= LPTMR_CSR_TCF_MASK;   // write 1 to TCF to clear the LPT timer compare flag

}

In the example I use LPTMR for 1 second interrupt; I have a file named vectors.c taken from the sample code. It declares an array and forces it to be allocated in the intvec segment:

#pragma location = ".intvec"

const vector_entry  __vector_table[] = //@ ".intvec" =

{

   VECTOR_000,           /* Initial SP           */

   VECTOR_001,           /* Initial PC           */

   VECTOR_002,

   VECTOR_003,

     ...

The entries VECTOR_*** are defined in vectors.h

#define VECTOR_000  (pointer*)__BOOT_STACK_ADDRESS   
#define VECTOR_001  __startup   
#define VECTOR_002  default_isr

you just have to substitue the right entry with your ISR. I'm working this way on KL15, KL25, K70 families.

Regards

Marco