IEC 60730 Safety Standard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEC 60730 Safety Standard

2,933 Views
ekasuwartadi
Contributor II

Dear all,

I would like to get functions (subroutines) for safety standard as described at IEC 60730 Safety Standard for Household Appliances . Are there people here whose experience to use or implement those functions ?

I have contacted technical customer support a few week ago but still do not get any answer yet.

Many thanks in advance !

Labels (1)
4 Replies

2,762 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Eka

you can download them from the following link:

APIEC60730: IEC 60730 Safety Standard for Household Appliances

under the name IEC60730B_KINETIS_SAFTY_HOUS-ROU:

Have a good day

Vicente

2,762 Views
ekasuwartadi
Contributor II

Thank you Vicente !

It requires approval from Freescale before downloading the file.

0 Kudos
Reply

2,762 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

You just need to log in on the freescale web page, like on the freescale community, read the software agreement and you can download the software.

Please let me know if you have any problem

Vicente  

0 Kudos
Reply

2,762 Views
ekasuwartadi
Contributor II

Thank a lot, Pedro !

I got the file now.

0 Kudos
Reply