IEC 60730 RAM test backup area

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEC 60730 RAM test backup area

Jump to solution
4,763 Views
MLapaj
Contributor II

Hi, 

I've got a question regarding RAM test functions from IEC60730 4.0 library for Cortex-M0+.

While using FS_CM0_RAM_AfterReset() and FS_CM0_RAM_Runtime() functions, can the tested memory area include the RAM test backup area or does the backup have to be excluded from tested addresses?

Let's suppose the tesed area is from 0x1FFFF000 to 0x20002FFF, which is the whole RAM area. Can the backup area overlap with tested area (e.g. can the backup area be placed at 0x1FFFF800 address, as long as it is reserved)?

0 Kudos
Reply
1 Solution
4,685 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @MLapaj 

I have received feedback on the matter.

The backup memory  should not be placed inside of tested SRAM memory range.

Our suggestion to test all the SRAM range is to create a least two test interfaces, where the backup memory (for the first instance) will be placed in the second instance memory range and vice versa.

Thank you for your patience.

Regards,

Diego

 

View solution in original post

6 Replies
4,746 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @MLapaj 

If the backup memory is inside the tested memory (ovelap),  the tests functions   probably  destroy the contents stored in the backup area for a certain block on a certain  in a iteration.  I will recommend to avoid overlapping.

Br,

Diego.

 

0 Kudos
Reply
4,720 Views
MLapaj
Contributor II

I don't mind the backup area contents being destroyed since it's reserved area anyway. What I am worried about is receiving false negative result of a test. Is there any chance of that happening? 

Or are there any other consequences to test area and backup area overlapping?

 

0 Kudos
Reply
4,708 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @MLapaj ,

 I will consult  internally  to validate my reply to your inquiry. Could you let me know  the MCU that you are plannig to use with the library?

Thank you,

Diego.

0 Kudos
Reply
4,702 Views
MLapaj
Contributor II

Hi @diego_charles, 

It's being used only on Kinetis KE06 at the time. 

0 Kudos
Reply
4,686 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @MLapaj 

I have received feedback on the matter.

The backup memory  should not be placed inside of tested SRAM memory range.

Our suggestion to test all the SRAM range is to create a least two test interfaces, where the backup memory (for the first instance) will be placed in the second instance memory range and vice versa.

Thank you for your patience.

Regards,

Diego

 

4,680 Views
MLapaj
Contributor II

I understand. Thank you for your help.

0 Kudos
Reply