I2S - K63

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2S - K63

1,295件の閲覧回数
anandkhandelwal
Contributor I

I have gone through few pdfs for I2S protocol there are few ICs which works on I2S but either those ICs work for specially speakers only or some ICs detect either mic or speaker and works accordingly.

There are few ICs also which works on both mic and speaker but they uses 2 different I2S ports for communication. I have not found any IC which can use a select signal and use same port for mic and speaker. Only WM8976 IC had this feature of use select input for speaker or mic but this IC is obsolete and company is closed.

So guide us how can we proceed further achieve above requirement. Also guide us for CAN interfacing on hardware.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,232件の閲覧回数
isaacavila
NXP Employee
NXP Employee

Hello Anand,

Unfortunately, I don't know which chip could serve you, we only use SGTL5000 or DA7212 in our examples.

About CAN reference you can consult Controller Area Network (CAN)|Freescale and/or CAN Physical Interfaces|Freescale  if your are interested on CAN transceivers.

I hope this can help you,

Best Regards,

Isaac

0 件の賞賛
返信