I2C to SPI Bridge

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C to SPI Bridge

I2C to SPI Bridge

  • Background:

NXP SC18IS602B I2C bus to SPI bridge chip is using TSSOP16 package, which is 16 leads; 0.65 mm pitch; 5 mm x 4.4 mm x 1.1 mm body. pastedImage_1.png

Customer requires to use a smaller package to emulate the SC18IS602B function.

Kinetis L series MKL03Z16VFK4R product uses QFN24 package with 4 mm x 4 mm x 0.58 mm body.

pastedImage_6.png

  • Demo Overview

The I2C to SPI Bridge demo provides a replacement solution demo of SC18IS602B chip. The demo is based on FRDM-KL03Z board using I2C0 module as I2C slave and SPI0 module as SPI master. Provided data buffer size is 400bytes. The demo software is based on KSDK V2.0 for FRDM-KL03Z software.

I2C slave interface:

Pin number                 Function              FRDM-KL03Z jumper

PTB3                          I2C0_SCL           J2-10

PTB4                          I2C0_SDA           J2-9

 

SPI master interface:

Pin number                 Function              FRDM-KL03Z jumper

PTA5                           SPI0_SS             J2_3

PTA6                           SPI0_MISO         J2_5

PTA7                           SPI0_MOSI         J2_4

PTB0                           SPI0_SCK           J2_6

 

INT pin (indicates if I2C to SPI Bridge allows i2c master start a new i2c transfer, low is active)

Pin number                 Function              FRDM-KL03Z jumper

PTB11                        GPIO output         J2_2

 

Connect I2C master with FRDM-KL03Z I2C slave interface and connect SPI slave with FRDM-KL03Z SPI master interface; Connect FRDM-KL03Z GND to I2C master and SPI slave before add power to those boards.  Below is the hardware platform connection way:

1.jpg

  • I2C to SPI Bridge Demo Function

For the KL03 chip with one SPI0_PCS0 chip select pin, I2C to SPI Bridge demo only supports function ID 0x01 as SPI write command.

For example: if i2c master want to write 8bytes (0x21,0x22...0x28) to SPI slave, the i2c master needs to send below data to FRDM-KL03Z board:  

[START] + [I2C Slave address+/W] + [0x01](Function ID) + [0x21](data 1) + [0x22](data 2) + ... +[0x28](data 8) + [STOP]  

 

I2C to SPI bridge demo supports Function ID 0xF0 to configure SPI interface: There provides four SPI baud rate: 6Mbps/3Mbps/1.5Mbps/1Mbps. More detailed info, please check below picture (picture abstracted from SC18IS602B datasheet):

For example: customer could configure SPI baud rate to 3Mbps with send below data to FRDM-KL03Z board:

       [START] + [I2C Slave address+/W] + [0Xf0](Function ID) + [0x01](data 1) + [STOP]

  • Hardware Platform

The demo is based on FRDM-KL03Z board, using internal IRC48M clock as system and bus clock source. There doesn’t need external clock source.

pastedImage_10.png

  • Toolchain supported

- IAR embedded Workbench 7.60.1  (Tested)

- Keil MDK 5.18a

- GCC ARM Embedded 2015-4.9-q3

- Kinetis Development Studio IDE 3.2.0

  • Running the Demo
  1. Connect a USB cable between the host PC and the USB port on the target board.
  2. Open a serial terminal with the following settings:

    - 9600 baud rate

    - 8 data bits

    - No parity

    - One stop bit

    - No flow control

  1. Download the program to the target board.
  2. I2C master start to configure SPI interface

     I2C to SPI bridge board I2C address is 0x7E.

1.jpg

  1. I2C master write data to SPI slave

   I2C master write 10bytes to SPI slave, it will send 11bytes (includes one function ID 0x01). The first data is 0xAA and the last data is 0x22.

   After I2C to SPI Bridge receive the data, it will send 10bytes to SPI slave.

  1.jpg

     I2C to SPI Bridge receive 10 bytes

1.jpg

1.jpg

    I2C to SPI Bridge send 10bytes to SPI slave

1.jpg

1.jpg

  1. I2C master read data from SPI slave

   I2C master read 10bytes(0x10 to 0x19) from SPI slave need to write data to SPI slave at first, then read data from I2C to SPI bridge data buffer directly.

   Here just shows read 10bytes from I2C to SPI bridge data buffer.

1.jpg

1.jpg

1.jpg

Attached I2C to SPI Bridge demo software default location is:

..\SDK_2.0_FRDM-KL03Z\boards\frdmkl03z\user_apps\i2c_to_spi

添付
コメント

Hello,

when I use the chip I can only send 12 IC2 bytes at once (Address + FunctionID + data).

If I send more than 12 Bytes the chip pull the clock low, but not back (clock stretching).

Sometimes I get no acknowledge for the IC.

The IC has a buffer of 200 bytes but I can use only 10 bytes.

On you pictures, I see that you send only 12 bytes. (you send only 10 data bytes).

Do you have the same issue like me?

Hi,

I had tested the data buffer with 400 bytes.

The I2C master send 400 bytes to I2C to SPI bridge without any problem, the SPI slave could get those 398 bytes sent from I2C master. 

best regards,

Mike

Hello,

how can you send 400bytes at once?

The chip has only a buffer of 200 bytes.

Hi,

I am using KL03 simulate the SC18IS602B chip and extend the data buffer to 400bytes.

Please check the i2c-to-spi code:

pastedImage_4.png

And I do a test to send 400 bytes from I2C master, which works normally as below pictures show:

pastedImage_5.png

pastedImage_7.png

pastedImage_8.png

pastedImage_6.png

pastedImage_13.png

I2C data start with 0x1, 0x21

pastedImage_9.png

I2C data stop with 0xad, 0xae, 0xaf

pastedImage_10.png

SPI master send data start with 0x21, 0x22 ... :

pastedImage_1.png

SPI master send data stop with 0xad, 0xae and 0xaf:

pastedImage_12.png

Thank you for the attention.


Have a great day,
Ma Hui

I can configure the chip but get no clock or data when i send address+functionid+data.  Any ideas would be welcome.  Im using arduino as controller.

Please check the SPI pins related configure.

I can configure this chip and it will run for some time and then it stops responding to I2C commands and the SPI bus appears to stop working correctly.  No MISO data and the clock rate changes from the 460 kHz that I set it to to 1.8 MHz.  Here is what the data looks like when it failsLogic Analyser screen shot.JPG

What's the SPI slave device you connected?

best regards,

Mike

%3CLINGO-SUB%20id%3D%22lingo-sub-1119464%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3EI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119464%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CUL%20style%3D%22list-style-type%3A%20square%3B%22%3E%3CLI%3EBackground%EF%BC%9A%3C%2FLI%3E%3C%2FUL%3E%3CP%20style%3D%22margin-left%3A%200.25in%3B%22%3ENXP%20SC18IS602B%20I2C%E3%83%90%E3%82%B9%E3%81%8B%E3%82%89SPI%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%83%81%E3%83%83%E3%83%97%E3%81%B8%E3%81%AETSSOP16%E3%83%91%E3%83%83%E3%82%B1%E3%83%BC%E3%82%B8%E3%80%81%E3%81%A4%E3%81%BE%E3%82%8A16%E3%83%AA%E3%83%BC%E3%83%89%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%820.65%20mm%E3%83%94%E3%83%83%E3%83%81%3B%E6%9C%AC%E4%BD%93%E3%81%AF5%20mm%20x%204.4%20mm%20x%201.1%20mm%E3%80%82%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_1.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_1.png%22%20style%3D%22width%3A%20200px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111462iBAFE03D0DBD07BA4%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_1.png%22%20alt%3D%22pastedImage_1.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_1.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%20.25in%3B%22%3E%E3%81%8A%E5%AE%A2%E6%A7%98%E3%81%AF%E3%80%81SC18IS602B%E6%A9%9F%E8%83%BD%E3%82%92%E3%82%A8%E3%83%9F%E3%83%A5%E3%83%AC%E3%83%BC%E3%83%88%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AB%E3%80%81%E3%82%88%E3%82%8A%E5%B0%8F%E3%81%95%E3%81%AA%E3%83%91%E3%83%83%E3%82%B1%E3%83%BC%E3%82%B8%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%20.25in%3B%22%3EKinetis%20L%E3%82%B7%E3%83%AA%E3%83%BC%E3%82%BAMKL03Z16VFK4R%E8%A3%BD%E5%93%81%E3%81%AF%E3%80%814mm%20x%204mm%20x%200.58mm%E3%81%AE%E3%83%9C%E3%83%87%E3%82%A3%E3%81%A7QFN24%E3%83%91%E3%83%83%E3%82%B1%E3%83%BC%E3%82%B8%E3%82%92%E6%8E%A1%E7%94%A8%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_6.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_6.png%22%20style%3D%22width%3A%20257px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111461i8736CFACD36B62B8%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_6.png%22%20alt%3D%22pastedImage_6.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_6.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CUL%20style%3D%22list-style-type%3A%20square%3B%22%3E%3CLI%3EDemo%20Overview%3C%2FLI%3E%3C%2FUL%3E%3CP%20style%3D%22margin-left%3A%20.25in%3B%22%3EI2C%20%E3%81%8B%E3%82%89%20SPI%20%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%81%AE%E3%83%87%E3%83%A2%E3%81%A7%E3%81%AF%E3%80%81SC18IS602B%20%E3%83%81%E3%83%83%E3%83%97%E3%81%AE%E4%BB%A3%E6%9B%BF%E3%82%BD%E3%83%AA%E3%83%A5%E3%83%BC%E3%82%B7%E3%83%A7%E3%83%B3%E3%81%AE%E3%83%87%E3%83%A2%E3%82%92%E6%8F%90%E4%BE%9B%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E3%81%93%E3%81%AE%E3%83%87%E3%83%A2%E3%81%AF%E3%80%81I2C0%E3%83%A2%E3%82%B8%E3%83%A5%E3%83%BC%E3%83%AB%E3%82%92I2C%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%A8%E3%81%97%E3%81%A6%E4%BD%BF%E7%94%A8%E3%81%97%E3%80%81SPI0%E3%83%A2%E3%82%B8%E3%83%A5%E3%83%BC%E3%83%AB%E3%82%92SPI%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%A8%E3%81%97%E3%81%A6%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8BFRDM-KL03Z%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AB%E5%9F%BA%E3%81%A5%E3%81%84%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%E6%8F%90%E4%BE%9B%E3%81%95%E3%82%8C%E3%82%8B%E3%83%87%E3%83%BC%E3%82%BF%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%E3%82%B5%E3%82%A4%E3%82%BA%E3%81%AF400%E3%83%90%E3%82%A4%E3%83%88%E3%81%A7%E3%81%99%E3%80%82%E3%83%87%E3%83%A2%E3%82%BD%E3%83%95%E3%83%88%E3%82%A6%E3%82%A7%E3%82%A2%E3%81%AF%E3%80%81KSDK%20V2.0%20for%20FRDM-KL03Z%E3%82%BD%E3%83%95%E3%83%88%E3%82%A6%E3%82%A7%E3%82%A2%E3%81%AB%E5%9F%BA%E3%81%A5%E3%81%84%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3EI2C%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%83%BC%E3%82%B9%3A%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3E%E3%83%94%E3%83%B3%E7%95%AA%E5%8F%B7%E6%A9%9F%E8%83%BDFRDM-KL03Z%E3%82%B8%E3%83%A3%E3%83%B3%E3%83%91%E3%83%BC%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3EPTB3%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20I2C0_SCL%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20J2-10%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3EPTB4%20I2C0_SDA%20J2-9%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%22%3E%26nbsp%3B%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3ESPI%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%83%BC%E3%82%B9%3A%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3E%E3%83%94%E3%83%B3%E7%95%AA%E5%8F%B7%E6%A9%9F%E8%83%BDFRDM-KL03Z%E3%82%B8%E3%83%A3%E3%83%B3%E3%83%91%E3%83%BC%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3EPTA5%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20SPI0_SS%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20J2_3%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3EPTA6%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20SPI0_MISO%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20J2_5%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3EPTA7%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20SPI0_MOSI%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20J2_4%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3EPTB0%20SPI0_SCK%20J2_6%3C%2FP%3E%3CBR%20%2F%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3EINT%E3%83%94%E3%83%B3(I2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%81%A7i2c%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%8C%E6%96%B0%E3%81%97%E3%81%84i2c%E8%BB%A2%E9%80%81%E3%82%92%E9%96%8B%E5%A7%8B%E3%81%A7%E3%81%8D%E3%82%8B%E3%81%8B%E3%81%A9%E3%81%86%E3%81%8B%E3%82%92%E7%A4%BA%E3%81%97%E3%80%81%E3%83%AD%E3%83%BC%E3%81%8C%E3%82%A2%E3%82%AF%E3%83%86%E3%82%A3%E3%83%96%E3%81%A7%E3%81%82%E3%82%8B%E3%81%93%E3%81%A8%E3%82%92%E7%A4%BA%E3%81%97%E3%81%BE%E3%81%99)%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3E%E3%83%94%E3%83%B3%E7%95%AA%E5%8F%B7%E6%A9%9F%E8%83%BDFRDM-KL03Z%E3%82%B8%E3%83%A3%E3%83%B3%E3%83%91%E3%83%BC%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3EPTB11%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%26nbsp%3B%20GPIO%20output%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%20%26nbsp%3B%26nbsp%3B%20J2_2%3C%2FP%3E%3CP%20style%3D%22margin-bottom%3A%20.0001pt%3B%20text-indent%3A%20.25in%3B%22%3E%26nbsp%3B%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%20.25in%3B%22%3EI2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%82%92FRDM-KL03Z%20I2C%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%83%BC%E3%82%B9%E3%81%AB%E6%8E%A5%E7%B6%9A%E3%81%97%E3%80%81SPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%82%92FRDM-KL03Z%20SPI%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%83%BC%E3%82%B9%E3%81%AB%E6%8E%A5%E7%B6%9A%E3%81%97%E3%81%BE%E3%81%99%E3%80%82FRDM-KL03Z%20GND%E3%82%92I2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%A8SPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%AB%E6%8E%A5%E7%B6%9A%E3%81%97%E3%81%A6%E3%81%8B%E3%82%89%E3%80%81%E3%81%93%E3%82%8C%E3%82%89%E3%81%AE%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AB%E9%9B%BB%E6%BA%90%E3%82%92%E8%BF%BD%E5%8A%A0%E3%81%97%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%E4%BB%A5%E4%B8%8B%E3%81%AF%E3%80%81%E3%83%8F%E3%83%BC%E3%83%89%E3%82%A6%E3%82%A7%E3%82%A2%E3%83%97%E3%83%A9%E3%83%83%E3%83%88%E3%83%95%E3%82%A9%E3%83%BC%E3%83%A0%E3%81%AE%E6%8E%A5%E7%B6%9A%E6%96%B9%E6%B3%95%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111460iECB164DB1D7D9169%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CUL%20style%3D%22list-style-type%3A%20square%3B%22%3E%3CLI%3EI2C%20to%20SPI%20Bridge%20%E3%83%87%E3%83%A2%E6%A9%9F%E8%83%BD%3C%2FLI%3E%3C%2FUL%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3ESPI0_PCS0%E3%83%81%E3%83%83%E3%83%97%E9%81%B8%E6%8A%9E%E3%83%94%E3%83%B3%E3%81%8C%201%20%E3%81%A4%E3%81%82%E3%82%8B%20KL03%20%E3%83%81%E3%83%83%E3%83%97%E3%81%AE%E5%A0%B4%E5%90%88%E3%80%81I2C%20to%20SPI%20Bridge%20%E3%83%87%E3%83%A2%E3%81%A7%E3%81%AF%E3%80%81SPI%20%E6%9B%B8%E3%81%8D%E8%BE%BC%E3%81%BF%E3%82%B3%E3%83%9E%E3%83%B3%E3%83%89%E3%81%A8%E3%81%97%E3%81%A6%E6%A9%9F%E8%83%BD%20ID%200x01%E3%81%AE%E3%81%BF%E3%81%8C%E3%82%B5%E3%83%9D%E3%83%BC%E3%83%88%E3%81%95%E3%82%8C%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%E4%BE%8B%3Ai2c%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%8C8%E3%83%90%E3%82%A4%E3%83%88(0x21%2C0x22...0x28)SPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%AB%E3%80%81i2c%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%AF%E4%BB%A5%E4%B8%8B%E3%81%AE%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92FRDM-KL03Z%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AB%E9%80%81%E4%BF%A1%E3%81%99%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%5BSTART%5D%20%2B%20%5BI2C%20Slave%20address%2B%2FW%5D%20%2B%20%5B0x01%5D(%E6%A9%9F%E8%83%BDID)%20%2B%20%5B0x21%5D(%E3%83%87%E3%83%BC%E3%82%BF1)%20%2B%20%5B0x22%5D(%E3%83%87%E3%83%BC%E3%82%BF2)%20%2B%20...%20%2B%5B0x28%5D(%E3%83%87%E3%83%BC%E3%82%BF8)%20%2B%20%5BSTOP%5D%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%26nbsp%3B%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%83%87%E3%83%A2%E3%81%AF%E3%80%81SPI%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%82%A4%E3%82%B9%E3%82%92%E6%A7%8B%E6%88%90%E3%81%99%E3%82%8B%E3%81%9F%E3%82%81%E3%81%AE%E6%A9%9F%E8%83%BDID%200xF0%E3%82%92%E3%82%B5%E3%83%9D%E3%83%BC%E3%83%88%E3%81%97%E3%81%BE%E3%81%99%3A6Mbps%20%2F%203Mbps%20%2F%201.5Mbps%20%2F%201Mbps%E3%81%AE4%E3%81%A4%E3%81%AESPI%E3%83%9C%E3%83%BC%E3%83%AC%E3%83%BC%E3%83%88%E3%82%92%E6%8F%90%E4%BE%9B%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E8%A9%B3%E7%B4%B0%E3%81%AB%E3%81%A4%E3%81%84%E3%81%A6%E3%81%AF%E3%80%81%E4%BB%A5%E4%B8%8B%E3%81%AE%E7%94%BB%E5%83%8F%E3%82%92%E7%A2%BA%E8%AA%8D%E3%81%97%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84(SC18IS602B%E3%83%87%E3%83%BC%E3%82%BF%E3%82%B7%E3%83%BC%E3%83%88%E3%81%8B%E3%82%89%E6%8A%9C%E7%B2%8B%E3%81%97%E3%81%9F%E7%94%BB%E5%83%8F)%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%E4%BE%8B%3A%E3%81%8A%E5%AE%A2%E6%A7%98%E3%81%AF%E3%80%81SPI%E3%83%9C%E3%83%BC%E3%83%AC%E3%83%BC%E3%83%88%E3%82%923Mbps%E3%81%AB%E6%A7%8B%E6%88%90%E3%81%97%E3%80%81%E4%BB%A5%E4%B8%8B%E3%81%AE%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92FRDM-KL03Z%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AB%E9%80%81%E4%BF%A1%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%5BSTART%5D%20%2B%20%5BI2C%20Slave%20address%2B%2FW%5D%20%2B%20%5B0Xf0%5D(%E6%A9%9F%E8%83%BDID)%20%2B%20%5B0x01%5D(%E3%83%87%E3%83%BC%E3%82%BF1)%20%2B%20%5BSTOP%5D%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CUL%20style%3D%22list-style-type%3A%20square%3B%22%3E%3CLI%3E%E3%83%8F%E3%83%BC%E3%83%89%E3%82%A6%E3%82%A7%E3%82%A2%E3%83%97%E3%83%A9%E3%83%83%E3%83%88%E3%83%95%E3%82%A9%E3%83%BC%E3%83%A0%3C%2FLI%3E%3C%2FUL%3E%3CP%20style%3D%22margin-left%3A%20.25in%3B%22%3E%E3%81%93%E3%81%AE%E3%83%87%E3%83%A2%E3%81%AFFRDM-KL03Z%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AB%E5%9F%BA%E3%81%A5%E3%81%84%E3%81%A6%E3%81%8A%E3%82%8A%E3%80%81%E5%86%85%E9%83%A8IRC48M%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E3%82%92%E3%82%B7%E3%82%B9%E3%83%86%E3%83%A0%E3%81%8A%E3%82%88%E3%81%B3%E3%83%90%E3%82%B9%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E3%82%BD%E3%83%BC%E3%82%B9%E3%81%A8%E3%81%97%E3%81%A6%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E5%A4%96%E9%83%A8%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E3%82%BD%E3%83%BC%E3%82%B9%E3%81%AF%E5%BF%85%E8%A6%81%E3%81%82%E3%82%8A%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin-left%3A%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_10.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_10.png%22%20style%3D%22width%3A%20576px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111459i0F12A3A243ECF620%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_10.png%22%20alt%3D%22pastedImage_10.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_10.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CUL%20style%3D%22list-style-type%3A%20square%3B%22%3E%3CLI%3E%E3%82%B5%E3%83%9D%E3%83%BC%E3%83%88%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8B%E3%83%84%E3%83%BC%E3%83%AB%E3%83%81%E3%82%A7%E3%83%BC%E3%83%B3%3C%2FLI%3E%3C%2FUL%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E-%20IAR%20embedded%20Workbench%207.60.1%20(%E8%8B%B1%E8%AA%9E)(%E3%83%86%E3%82%B9%E3%83%88%E6%B8%88%E3%81%BF)%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E-%20%E3%82%AD%E3%83%BC%E3%83%ABMDK%205.18a%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E-%20GCC%20ARM%20%E7%B5%84%E3%81%BF%E8%BE%BC%E3%81%BF%202015-4.9-q3%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E-%20Kinetis%20Development%20Studio%20IDE%203.2.0%20(%E8%8B%B1%E8%AA%9E)%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CUL%20style%3D%22list-style-type%3A%20square%3B%22%3E%3CLI%3E%E3%83%87%E3%83%A2%E3%81%AE%E5%AE%9F%E8%A1%8C%3C%2FLI%3E%3C%2FUL%3E%3COL%3E%3CLI%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%E3%83%9B%E3%82%B9%E3%83%88PC%E3%81%A8%E3%82%BF%E3%83%BC%E3%82%B2%E3%83%83%E3%83%88%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AEUSB%E3%83%9D%E3%83%BC%E3%83%88%E3%82%92USB%E3%82%B1%E3%83%BC%E3%83%96%E3%83%AB%E3%81%A7%E6%8E%A5%E7%B6%9A%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FLI%3E%3CLI%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%E6%AC%A1%E3%81%AE%E8%A8%AD%E5%AE%9A%E3%81%A7%E3%82%B7%E3%83%AA%E3%82%A2%E3%83%AB%E7%AB%AF%E6%9C%AB%E3%82%92%E9%96%8B%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FLI%3E%3C%2FOL%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E-%209600%E3%83%9C%E3%83%BC%E3%83%AC%E3%83%BC%E3%83%88%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E-%208%E3%83%87%E3%83%BC%E3%82%BF%E3%83%93%E3%83%83%E3%83%88%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E-%20%E3%83%91%E3%83%AA%E3%83%86%E3%82%A3%E3%81%AA%E3%81%97%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E-%201%E3%82%B9%E3%83%88%E3%83%83%E3%83%97%E3%83%93%E3%83%83%E3%83%88%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E-%20%E3%83%95%E3%83%AD%E3%83%BC%E5%88%B6%E5%BE%A1%E3%81%AA%E3%81%97%3C%2FP%3E%3COL%20start%3D%223%22%3E%3CLI%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%E3%83%97%E3%83%AD%E3%82%B0%E3%83%A9%E3%83%A0%E3%82%92%E3%82%BF%E3%83%BC%E3%82%B2%E3%83%83%E3%83%88%E3%83%9C%E3%83%BC%E3%83%89%E3%81%AB%E3%83%80%E3%82%A6%E3%83%B3%E3%83%AD%E3%83%BC%E3%83%89%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FLI%3E%3CLI%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%8C%E8%B5%B7%E5%8B%95%E3%81%97%E3%81%A6SPI%E3%82%A4%E3%83%B3%E3%82%BF%E3%83%BC%E3%83%95%E3%82%A7%E3%83%BC%E3%82%B9%E3%82%92%E8%A8%AD%E5%AE%9A%3C%2FLI%3E%3C%2FOL%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%83%9C%E3%83%BC%E3%83%89I2C%E3%82%A2%E3%83%89%E3%83%AC%E3%82%B9%E3%81%AF0x7E%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111458i4A1CAE02330AFE9C%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3COL%20start%3D%225%22%3E%3CLI%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%8CSPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%AB%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E6%9B%B8%E3%81%8D%E8%BE%BC%E3%81%BF%E3%81%BE%E3%81%99%3C%2FLI%3E%3C%2FOL%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%AFSPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%AB10%E3%83%90%E3%82%A4%E3%83%88%E3%82%92%E6%9B%B8%E3%81%8D%E8%BE%BC%E3%81%BF%E3%80%8111%E3%83%90%E3%82%A4%E3%83%88%E3%82%92%E9%80%81%E4%BF%A1%E3%81%97%E3%81%BE%E3%81%99(%E6%A9%9F%E8%83%BDID%E3%81%8C1%E3%81%A40x01%E5%90%AB%E3%81%BE%E3%82%8C%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99)%E3%80%82%E6%9C%80%E5%88%9D%E3%81%AE%E3%83%87%E3%83%BC%E3%82%BF%E3%81%AF0xAA%E3%81%95%E3%82%8C%E3%80%81%E6%9C%80%E5%BE%8C%E3%81%AE%E3%83%87%E3%83%BC%E3%82%BF%E3%81%AF0x22%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%20to%20SPI%20Bridge%E3%81%8C%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E5%8F%97%E4%BF%A1%E3%81%97%E3%81%9F%E5%BE%8C%E3%80%81SPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%AB10%E3%83%90%E3%82%A4%E3%83%88%E3%82%92%E9%80%81%E4%BF%A1%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%26nbsp%3B%20%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F12421i86EA298A4832D717%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%81%AF10%E3%83%90%E3%82%A4%E3%83%88%E3%82%92%E5%8F%97%E4%BF%A1%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111457iAD50525A14E647EB%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111456i32C85811FF4DE357%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%20%E3%81%8B%E3%82%89%20SPI%20%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%81%A7%2010%20%E3%83%90%E3%82%A4%E3%83%88%E3%82%92%20SPI%20%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%AB%E9%80%81%E4%BF%A1%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111455i8D313E55EDCD4E3B%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111454iC2D5DEC54DE39A2C%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3COL%20start%3D%226%22%3E%3CLI%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%AFSPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%8B%E3%82%89%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E8%AA%AD%E3%81%BF%E5%87%BA%E3%81%97%E3%81%BE%E3%81%99%3C%2FLI%3E%3C%2FOL%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3EI2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%AF%E3%80%81SPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%8B%E3%82%8910%E3%83%90%E3%82%A4%E3%83%88(0x10%E3%80%9C0x19)%E3%82%92%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81%E6%9C%80%E5%88%9D%E3%81%ABSPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%AB%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E6%9B%B8%E3%81%8D%E8%BE%BC%E3%82%93%E3%81%A7%E3%81%8B%E3%82%89%E3%80%81I2C%E3%81%8B%E3%82%89SPI%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%83%87%E3%83%BC%E3%82%BF%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%E3%81%AB%E7%9B%B4%E6%8E%A5%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%8B%E5%BF%85%E8%A6%81%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%E3%81%93%E3%81%93%E3%81%A7%E3%81%AF%E3%80%81I2C%E3%81%8B%E3%82%89SPI%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%83%87%E3%83%BC%E3%82%BF%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%E3%81%B8%E3%81%AE10%E3%83%90%E3%82%A4%E3%83%88%E3%81%AE%E8%AA%AD%E3%81%BF%E5%8F%96%E3%82%8A%E3%82%92%E7%A4%BA%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111453i9DB310DE861DF437%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F12684i51694FFF133D19EB%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%221.jpg%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F111452iD79026D34565C315%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%221.jpg%22%20alt%3D%221.jpg%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3E1.jpg%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3ESPI%20Bridge%E3%83%87%E3%83%A2%E3%83%BB%E3%82%BD%E3%83%95%E3%83%88%E3%82%A6%E3%82%A7%E3%82%A2%E3%81%AB%E6%B7%BB%E4%BB%98%E3%81%95%E3%82%8C%E3%81%A6%E3%81%84%E3%82%8BI2C%E3%81%AE%E3%83%87%E3%83%95%E3%82%A9%E3%83%AB%E3%83%88%E3%81%AE%E5%A0%B4%E6%89%80%E3%81%AF%E6%AC%A1%E3%81%AE%E3%81%A8%E3%81%8A%E3%82%8A%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CP%20style%3D%22margin%3A%200in%200in%20.0001pt%20.25in%3B%22%3E..%5CSDK_2.0_FRDM-KL03Z%5C%E3%83%9C%E3%83%BC%E3%83%89%5Cfrdmkl03z%5Cuser_apps%5Ci2c_to_spi%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-LABS%20id%3D%22lingo-labs-1119464%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CLINGO-LABEL%3EFreedom%E9%96%8B%E7%99%BA%E3%83%97%E3%83%A9%E3%83%83%E3%83%88%E3%83%95%E3%82%A9%E3%83%BC%E3%83%A0%3C%2FLINGO-LABEL%3E%3CLINGO-LABEL%3EKinetis%20L%E3%82%B7%E3%83%AA%E3%83%BC%E3%82%BA%E3%83%BB%E3%83%9E%E3%82%A4%E3%82%AF%E3%83%AD%E3%82%B3%E3%83%B3%E3%83%88%E3%83%AD%E3%83%BC%E3%83%A9%3C%2FLINGO-LABEL%3E%3C%2FLINGO-LABS%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1119472%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E6%97%A5%E6%99%82%3AI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119472%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3E%E6%8E%A5%E7%B6%9A%E3%81%97%E3%81%9FSPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%83%87%E3%83%90%E3%82%A4%E3%82%B9%E3%81%AF%E4%BD%95%E3%81%A7%E3%81%99%E3%81%8B%3F%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%82%88%E3%82%8D%E3%81%97%E3%81%8F%E3%81%8A%E9%A1%98%E3%81%84%E3%81%84%E3%81%9F%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3EMike%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1119471%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E6%97%A5%E6%99%82%3AI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119471%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3E%E3%81%93%E3%81%AE%E3%83%81%E3%83%83%E3%83%97%E3%82%92%E6%A7%8B%E6%88%90%E3%81%A7%E3%81%8D%E3%80%81%E3%81%97%E3%81%B0%E3%82%89%E3%81%8F%E3%81%AE%E9%96%93%E5%8B%95%E4%BD%9C%E3%81%97%E3%80%81%E3%81%9D%E3%81%AE%E5%BE%8C%E3%80%81I2C%E3%82%B3%E3%83%9E%E3%83%B3%E3%83%89%E3%81%B8%E3%81%AE%E5%BF%9C%E7%AD%94%E3%82%92%E5%81%9C%E6%AD%A2%E3%81%97%E3%80%81SPI%E3%83%90%E3%82%B9%E3%81%8C%E6%AD%A3%E3%81%97%E3%81%8F%E5%8B%95%E4%BD%9C%E3%81%97%E3%81%AA%E3%81%8F%E3%81%AA%E3%81%A3%E3%81%9F%E3%82%88%E3%81%86%E3%81%AB%E8%A6%8B%E3%81%88%E3%81%BE%E3%81%99%E3%80%82MISO%20%E3%83%87%E3%83%BC%E3%82%BF%E3%81%AF%E3%81%AA%E3%81%8F%E3%80%81%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%20%E3%83%AC%E3%83%BC%E3%83%88%E3%81%AF%E8%A8%AD%E5%AE%9A%E3%81%97%E3%81%9F%20460%20kHz%20%E3%81%8B%E3%82%89%201.8%20MHz%20%E3%81%AB%E5%A4%89%E5%8C%96%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%E5%A4%B1%E6%95%97%E3%81%97%E3%81%9F%E5%A0%B4%E5%90%88%E3%81%AE%E3%83%87%E3%83%BC%E3%82%BF%E3%81%AF%E6%AC%A1%E3%81%AE%E3%82%88%E3%81%86%E3%81%AB%E3%81%AA%E3%82%8A%E3%81%BE%E3%81%99%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22Logic%20Analyser%20screen%20shot.JPG%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22Logic%20Analyser%20screen%20shot.JPG%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F22298i0B918FF122111290%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22Logic%20Analyser%20screen%20shot.JPG%22%20alt%3D%22Logic%20Analyser%20screen%20shot.JPG%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3ELogic%20Analyser%20screen%20shot.JPG%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1119470%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E6%97%A5%E6%99%82%3AI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119470%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3ESPI%E3%83%94%E3%83%B3%E9%96%A2%E9%80%A3%E3%81%AE%E6%A7%8B%E6%88%90%E3%82%92%E7%A2%BA%E8%AA%8D%E3%81%97%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1119469%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E6%97%A5%E6%99%82%3AI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119469%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3E%E3%83%81%E3%83%83%E3%83%97%E3%82%92%E8%A8%AD%E5%AE%9A%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81%E3%82%A2%E3%83%89%E3%83%AC%E3%82%B9%2B%20functionid%20%2B%20data%E3%82%92%E9%80%81%E4%BF%A1%E3%81%99%E3%82%8B%E3%81%A8%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E3%82%84%E3%83%87%E3%83%BC%E3%82%BF%E3%81%8C%E5%BE%97%E3%82%89%E3%82%8C%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%E3%81%A9%E3%82%93%E3%81%AA%E3%82%A2%E3%82%A4%E3%83%87%E3%82%A2%E3%81%A7%E3%82%82%E5%A4%A7%E6%AD%93%E8%BF%8E%E3%81%A7%E3%81%99%E3%80%82%E7%A7%81%E3%81%AF%E3%82%B3%E3%83%B3%E3%83%88%E3%83%AD%E3%83%BC%E3%83%A9%E3%83%BC%E3%81%A8%E3%81%97%E3%81%A6arduino%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1119468%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E6%97%A5%E6%99%82%3AI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119468%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EHi%2C%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3EKL03%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%97%E3%81%A6SC18IS602B%E3%83%81%E3%83%83%E3%83%97%E3%82%92%E3%82%B7%E3%83%9F%E3%83%A5%E3%83%AC%E3%83%BC%E3%83%88%E3%81%97%E3%80%81%E3%83%87%E3%83%BC%E3%82%BF%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%E3%82%92400%E3%83%90%E3%82%A4%E3%83%88%E3%81%AB%E6%8B%A1%E5%BC%B5%E3%81%97%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3Ei2c-to-spi%20%E3%82%B3%E3%83%BC%E3%83%89%E3%82%92%E7%A2%BA%E8%AA%8D%E3%81%97%E3%81%A6%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%E3%80%82%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_4.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_4.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F24856iF65F752E014F2302%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_4.png%22%20alt%3D%22pastedImage_4.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_4.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%E3%81%9D%E3%81%97%E3%81%A6%E3%80%81I2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%8B%E3%82%89400%E3%83%90%E3%82%A4%E3%83%88%E3%82%92%E9%80%81%E4%BF%A1%E3%81%99%E3%82%8B%E3%83%86%E3%82%B9%E3%83%88%E3%82%92%E8%A1%8C%E3%81%84%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81%E3%81%93%E3%82%8C%E3%81%AF%E4%BB%A5%E4%B8%8B%E3%81%AE%E5%86%99%E7%9C%9F%E3%81%AB%E7%A4%BA%E3%81%99%E3%82%88%E3%81%86%E3%81%AB%E6%AD%A3%E5%B8%B8%E3%81%AB%E5%8B%95%E4%BD%9C%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_5.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_5.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F24802iF59F3E91EAB2F08D%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_5.png%22%20alt%3D%22pastedImage_5.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_5.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_7.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_7.png%22%20style%3D%22width%3A%20584px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F24855i1569505A7B1D80BD%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_7.png%22%20alt%3D%22pastedImage_7.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_7.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_8.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_8.png%22%20style%3D%22width%3A%20344px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F24877i20B00B0FCE925473%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_8.png%22%20alt%3D%22pastedImage_8.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_8.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_6.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_6.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F24590i822B440580F25132%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_6.png%22%20alt%3D%22pastedImage_6.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_6.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_13.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_13.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F25057i025984880A0865D1%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_13.png%22%20alt%3D%22pastedImage_13.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_13.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3EI2C%E3%83%87%E3%83%BC%E3%82%BF%E3%81%AF0x1%E3%81%8B%E3%82%89%E5%A7%8B%E3%81%BE%E3%82%8A%E3%81%BE%E3%81%990x21%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_9.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_9.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F24915i1A55CDCE9C73714F%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_9.png%22%20alt%3D%22pastedImage_9.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_9.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3EI2C%E3%83%87%E3%83%BC%E3%82%BF%E5%81%9C%E6%AD%A2(0xad%E3%80%810xae%E3%80%810xaf)%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_10.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_10.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F24958i34F8567B7A3EB012%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_10.png%22%20alt%3D%22pastedImage_10.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_10.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3ESPI%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E9%80%81%E4%BF%A1%E3%83%87%E3%83%BC%E3%82%BF%E3%81%AF0x21%E3%80%810x22...%E3%81%A7%E5%A7%8B%E3%81%BE%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_1.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_1.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F25101i81009910158F7874%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_1.png%22%20alt%3D%22pastedImage_1.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_1.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3ESPI%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%AF%E3%80%810xad%E3%80%810xae%E3%80%81%E3%81%8A%E3%82%88%E3%81%B30xaf%E3%81%A7%E3%83%87%E3%83%BC%E3%82%BF%E3%82%92%E5%81%9C%E6%AD%A2%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3CSPAN%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_12.png%22%3E%3Cspan%20class%3D%22lia-inline-image-display-wrapper%22%20image-alt%3D%22pastedImage_12.png%22%20style%3D%22width%3A%20999px%3B%22%3E%3Cimg%20src%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fimage%2Fserverpage%2Fimage-id%2F25011iD76E1E506A4F02EB%2Fimage-size%2Flarge%3Fv%3Dv2%26amp%3Bpx%3D999%22%20role%3D%22button%22%20title%3D%22pastedImage_12.png%22%20alt%3D%22pastedImage_12.png%22%20%2F%3E%3Cspan%20class%3D%22lia-inline-image-caption%22%20onclick%3D%22event.preventDefault()%3B%22%3EpastedImage_12.png%3C%2Fspan%3E%3C%2Fspan%3E%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%81%94%E6%B8%85%E8%81%B4%E3%81%82%E3%82%8A%E3%81%8C%E3%81%A8%E3%81%86%E3%81%94%E3%81%96%E3%81%84%E3%81%BE%E3%81%97%E3%81%9F%E3%80%82%3C%2FP%3E%3CP%3E%3CBR%20%2F%3E%E8%89%AF%E3%81%84%E6%97%A5%E3%82%92%E3%81%8A%E9%81%8E%E3%81%94%E3%81%97%E3%81%8F%E3%81%A0%E3%81%95%E3%81%84%3CBR%20%2F%3E%E9%A6%AC%E6%85%A7(%E3%83%9E%E3%83%BB%E3%83%9B%E3%82%A4)%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1119467%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E6%97%A5%E6%99%82%3AI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119467%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EHello%2C%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%81%A9%E3%81%86%E3%81%99%E3%82%8C%E3%81%B0%E4%B8%80%E5%BA%A6%E3%81%AB400%E3%83%90%E3%82%A4%E3%83%88%E3%82%92%E9%80%81%E4%BF%A1%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%81%8B%3F%3C%2FP%3E%3CP%3E%E3%83%81%E3%83%83%E3%83%97%E3%81%AB%E3%81%AF%20200%20%E3%83%90%E3%82%A4%E3%83%88%E3%81%AE%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%E3%81%97%E3%81%8B%E3%81%82%E3%82%8A%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1119466%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E6%97%A5%E6%99%82%3AI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119466%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EHi%2C%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E7%A7%81%E3%81%AF400%E3%83%90%E3%82%A4%E3%83%88%E3%81%A7%E3%83%87%E3%83%BC%E3%82%BF%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%E3%82%92%E3%83%86%E3%82%B9%E3%83%88%E3%81%97%E3%81%BE%E3%81%97%E3%81%9F%E3%80%82%3C%2FP%3E%3CP%3EI2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%AF%E5%95%8F%E9%A1%8C%E3%81%AA%E3%81%8FI2C%E3%81%8B%E3%82%89SPI%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%E3%81%AB400%E3%83%90%E3%82%A4%E3%83%88%E3%82%92%E9%80%81%E4%BF%A1%E3%81%97%E3%80%81SPI%E3%82%B9%E3%83%AC%E3%83%BC%E3%83%96%E3%81%AFI2C%E3%83%9E%E3%82%B9%E3%82%BF%E3%83%BC%E3%81%8B%E3%82%89%E9%80%81%E4%BF%A1%E3%81%95%E3%82%8C%E3%81%9F398%E3%83%90%E3%82%A4%E3%83%88%E3%82%92%E5%8F%96%E5%BE%97%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%82%88%E3%82%8D%E3%81%97%E3%81%8F%E3%81%8A%E9%A1%98%E3%81%84%E3%81%84%E3%81%9F%E3%81%97%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3EMike%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1119465%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E6%97%A5%E6%99%82%3AI2C%E3%81%8B%E3%82%89SPI%E3%81%B8%E3%81%AE%E3%83%96%E3%83%AA%E3%83%83%E3%82%B8%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1119465%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%26lt%3Bmeta%20http-equiv%3D%22Content-Type%22%20content%3D%22text%2Fhtml%3B%20charset%3Dutf-8%22%20%2F%26gt%3B%0A%3CP%3EHello%2C%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%83%81%E3%83%83%E3%83%97%E3%82%92%E4%BD%BF%E7%94%A8%E3%81%99%E3%82%8B%E3%81%A8%E3%80%81%E4%B8%80%E5%BA%A6%E3%81%AB%E9%80%81%E4%BF%A1%E3%81%A7%E3%81%8D%E3%82%8BIC2%E3%83%90%E3%82%A4%E3%83%88%E3%81%AF12%E3%83%90%E3%82%A4%E3%83%88(%E3%82%A2%E3%83%89%E3%83%AC%E3%82%B9%2BFunctionID%20%2B%E3%83%87%E3%83%BC%E3%82%BF)%E3%81%AE%E3%81%BF%E3%81%A7%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3E12%E3%83%90%E3%82%A4%E3%83%88%E4%BB%A5%E4%B8%8A%E3%82%92%E9%80%81%E4%BF%A1%E3%81%99%E3%82%8B%E3%81%A8%E3%80%81%E3%83%81%E3%83%83%E3%83%97%E3%81%AF%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E3%82%92%E3%83%AD%E3%83%BC%E3%81%AB%E3%83%97%E3%83%AB%E3%81%97%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81%E6%88%BB%E3%81%99%E3%81%93%E3%81%A8%E3%81%AF%E3%81%82%E3%82%8A%E3%81%BE%E3%81%9B%E3%82%93(%E3%82%AF%E3%83%AD%E3%83%83%E3%82%AF%E3%82%B9%E3%83%88%E3%83%AC%E3%83%83%E3%83%81)%E3%80%82%3C%2FP%3E%3CP%3E%E6%99%82%E3%80%85%E3%80%81IC%E3%81%AB%E5%AF%BE%E3%81%97%E3%81%A6%E6%89%BF%E8%AA%8D%E3%81%8C%E5%B1%8A%E3%81%8B%E3%81%AA%E3%81%84%E3%81%93%E3%81%A8%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82%3C%2FP%3E%3CP%3EIC%E3%81%AB%E3%81%AF200%E3%83%90%E3%82%A4%E3%83%88%E3%81%AE%E3%83%90%E3%83%83%E3%83%95%E3%82%A1%E3%81%8C%E3%81%82%E3%82%8A%E3%81%BE%E3%81%99%E3%81%8C%E3%80%81%E7%A7%81%E3%81%AF10%E3%83%90%E3%82%A4%E3%83%88%E3%81%97%E3%81%8B%E4%BD%BF%E7%94%A8%E3%81%A7%E3%81%8D%E3%81%BE%E3%81%9B%E3%82%93%E3%80%82%3C%2FP%3E%3CP%3E%3C%2FP%3E%3CP%3E%E3%81%82%E3%81%AA%E3%81%9F%E3%81%AE%E5%86%99%E7%9C%9F%E3%81%A7%E3%81%AF%E3%80%8112%E3%83%90%E3%82%A4%E3%83%88%E3%81%97%E3%81%8B%E9%80%81%E4%BF%A1%E3%81%97%E3%81%A6%E3%81%84%E3%81%AA%E3%81%84%E3%81%93%E3%81%A8%E3%81%8C%E3%82%8F%E3%81%8B%E3%82%8A%E3%81%BE%E3%81%99%E3%80%82(10%20%E3%83%87%E3%83%BC%E3%82%BF%20%E3%83%90%E3%82%A4%E3%83%88%E3%81%AE%E3%81%BF%E3%82%92%E9%80%81%E4%BF%A1%E3%81%97%E3%81%BE%E3%81%99)%E3%80%82%3C%2FP%3E%3CP%3E%E3%81%82%E3%81%AA%E3%81%9F%E3%82%82%E7%A7%81%E3%81%A8%E5%90%8C%E3%81%98%E5%95%8F%E9%A1%8C%E3%82%92%E6%8A%B1%E3%81%88%E3%81%A6%E3%81%84%E3%81%BE%E3%81%99%E3%81%8B%3F%3C%2FP%3E%3C%2FLINGO-BODY%3E
評価なし
バージョン履歴
最終更新日:
‎01-22-2017 07:36 PM
更新者: