I2C on MKL15

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2C on MKL15

1,574 次查看
serjnone
Contributor I

Hi.

I have some problems witch i2c on mkl15z128.

I try to communicate with RTC DS1338. For beginning i try get on the bug START condition, Slave address write and STOP condition.

But i have problems.

I use PTE0/TPE1 GPIO pins.

My init function

void init_I2C(void)

{

    SIM_SCGC4 |= SIM_SCGC4_I2C1_MASK; //Turn on clock to I2C1 module

    SIM_SCGC5 |= SIM_SCGC5_PORTE_MASK;

    /* configure GPIO for I2C1 function */

    PORTE_PCR0 = PORT_PCR_ISF_MASK | PORT_PCR_MUX(6);

    PORTE_PCR1 = PORT_PCR_ISF_MASK | PORT_PCR_MUX(6);

    

    I2C1_F = I2C_F_ICR(14) | I2C_F_MULT(0);

    I2C1_C1 = I2C_C1_IICEN_MASK;

}

My functions for write i take from examples

void i2c_Wait(void)

{

  while((I2C1_S & I2C_S_IICIF_MASK)==0)

  {

    wdtFeed();

  }

  I2C1_S |= I2C_S_IICIF_MASK;

}

void IIC_StartTransmission (unsigned char SlaveID, unsigned char Mode)

{

  if(Mode == MWSR)

  {

    /* set transmission mode */

    MasterTransmission = MWSR;

  }

  else

  {

    /* set transmission mode */

    MasterTransmission = MRSW;

  }

  /* shift ID in right possition */

  SlaveID = (unsigned char) MMA7660_I2C_ADDRESS << 1;

  /* Set R/W bit at end of Slave Address */

  SlaveID |= (unsigned char)MasterTransmission;

  /* send start signal */

  i2c_Start();

  /* send ID with W/R bit */

  i2c_write_byte(SlaveID);

}

void MMA7660WriteRegister(unsigned char u8RegisterAddress, unsigned char u8Data)

{

  /* send data to slave */

  IIC_StartTransmission(SlaveID,MWSR);

  i2c_Wait();

  /* Send I2C address */

  I2C1_D = u8RegisterAddress;

  i2c_Wait();

  /* Send data */

  I2C1_D = u8Data;

  i2c_Wait();

  i2c_Stop();

  //Pause();

}

When i call MMA7660WriteRegister(0x1, 0x2) i have reboot device by WDT.

When i insert wdtFeed in while loop i have no reboot.

  while((I2C1_S & I2C_S_IICIF_MASK)==0)

  {

    wdtFeed();

  }

I have START condition but in I2C1_S i have no I2C_S_IICIF_MASK after START.

I have no idea what i do wrong. Pleas help me.

标签 (1)
0 项奖励
回复
2 回复数

1,331 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello serj none:

I assume you have pullup resistors in SCL and SDA lines, correct?

I would recommend checking the bus with an oscilloscope or logic analyzer. The IICIF flag should set as soon as 9 clock cycles are shifted out (8-bit data + ack/nack). The flag should set disregarding if the slave responds or not.

And some observations about your code:

- You are using I2C1 (not I2C0). Just double check that i2c_start(), i2c_write_byte() and i2c_Stop() functions refer to this I2C module instance.

- For address cycle the bit I2C1_C1[TX] should be set to '1', indicating Transmit mode. I do not see this in your code.

- Your function IIC_StartTransmission receives SlaveID as parameter, but then completely ignores such value and overwrites it with MMA7660_I2C_ADDRESS. Verify that you use the correct address for your RTC slave device.

I hope these comments help.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,331 次查看
serjnone
Contributor I

Thank you.

There are was shoted SCL and SCK lines.

I use i2c_1 and all fanctions referred to i2c_1.

I think examples from IAR not fully corrected.

After simple code i2s_start() in my project dos not work - a wrong slave address transmitted.

But if i write

i2c_start();

while((I2C1_S & (1<<5)) == 0); //waite while BUSY bit set

in any cases transmit correct slave address.

Also I change i2c_stop() :

i2c_stop();

while((I2C1_S & (1<<5)) != 0); //waite while BUSY bit clear

Now my code work stable and relable.

Thank you fo help.

0 项奖励
回复