I2C on K66F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,680件の閲覧回数
a8Chcx
Contributor V

Hi,

I am using K66F MCU for my controller.

My question: What is the voltage level allowed for I2C pins? Can I use the pull-up resisters to 5VDC on SDA and SCL? Or I have to use 3.3VDC for pull-up?

Thanks,

Christie

0 件の賞賛
返信
1 解決策
1,651件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @a8Chcx 

I recommend you to use a pullup to 3.3V, the FRDM-K66 uses 3.3V pullups with the ACCELEROMETER AND MAGNETOMETER internal sensors.

Best Regards, Miguel.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,652件の閲覧回数
Miguel04
NXP TechSupport
NXP TechSupport

Hi @a8Chcx 

I recommend you to use a pullup to 3.3V, the FRDM-K66 uses 3.3V pullups with the ACCELEROMETER AND MAGNETOMETER internal sensors.

Best Regards, Miguel.

0 件の賞賛
返信