I2C interface of ALS Sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C interface of ALS Sensor

3,032件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

     Generally,How to write to a register in ISL29023(ALS Sensor) throught I2C ?  Any examples codes aare there for that with respect to KEA-128???

5 返答(返信)

2,676件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH BALAJI,

    About how to write the ALS SENSOR register, you should read the the ALS sensor datasheet, to get the command, then use the I2C to send the according command to write the sensor.

  What we can give you is just the KEA128 I2C driver, for the detail application, you need to write the code by yourself.

  Please find the KEA128 i2c driver from the attachment

Wish it helps you!

If you still have question, please contact with me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,676件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi,

In the I2C driver the baud rate is kept as 0x1F ,what is the baud rate

that corresponds to?

On Thu, Mar 31, 2016 at 8:48 AM, kerryzhou <[email protected]>

0 件の賞賛
返信

2,676件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi VIGNESH,

      i2c baud rate is the I2C clk communication baud rate, you also can configure the baudrate which you want.

    For details, please check the KEA referece manual, I2Cx_F register.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,676件の閲覧回数
vigneshbalaji
Senior Contributor I

Hi Jing,

Can you please tell me,what does this 0x1F refer to that is it

corresponds to what baud rate???In the I2C driver we are putting it as 0x1F.

On Tue, Apr 5, 2016 at 2:59 PM, kerryzhou <[email protected]>

0 件の賞賛
返信

2,676件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Vignesh,

Could you tell me what the 0X1F from? Did you define the I2Cx_F=0x1f?

If yes, now I tell you how to calculate the baud rate.

I2C baud rate = I2C module clock speed (Hz)/(mul × SCL divider)

2C module clock speed is the bus clock.

mul=I2Cx_F[MULT]+1;

SCL divider, you need to check the Table 31-41. I2C divider and hold values in the KEA referece manual.

Now take I2Cx_F=0x1f as an example, it means, mul=1, SCL divider= 240.

47.jpg

Then, assume your bus clock=24Mhz,

I2C baud rate = 24Mhz/(1*240)=100Kbps.

More details, please read the referece manual carefully!

Wish it helps you!


Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信