I2C compentent stop bit control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C compentent stop bit control

1,783 Views
gordongao
Contributor II

I use i2c0 compentent,How can I control the stop bit, 

I change "LDD_I2C_SEND_STOP" to "LDD_I2C_NO_SEND_STOP" flag ,but only will sent out stop bit.

Thanks!

code:

uint8_t GI2C1_ReadAddress(uint8_t i2cAddr, uint8_t *memAddr, uint8_t memAddrSize, uint8_t *data, uint16_t dataSize)
{
uint8_t res = ERR_OK;

if (GI2C1_SelectSlave(i2cAddr)!=ERR_OK) {
return ERR_FAILED;
}
for(;;) { /* breaks */
if(memAddr!=NULL) { /* only if we want to send an address */
/* send device address and memory address */
GI2C1_deviceData.dataTransmittedFlg = FALSE;
res = CI2C1_MasterSendBlock(GI2C1_deviceData.handle, memAddr, memAddrSize, LDD_I2C_NO_SEND_STOP);
if (res!=ERR_OK) {
break; /* break for(;;) */
}
}
do { /* Wait until data is sent */
} while (!GI2C1_deviceData.dataTransmittedFlg);
/* receive data */
GI2C1_deviceData.dataReceivedFlg = FALSE;
res = CI2C1_MasterReceiveBlock(GI2C1_deviceData.handle, data, dataSize, LDD_I2C_NO_SEND_STOP);// LDD_I2C_SEND_STOP);
if (res!=ERR_OK) {
break; /* break for(;;) */
}
do
{ /* Wait until data is received */
} while (!GI2C1_deviceData.dataReceivedFlg);
break; /* break for(;;) */
} /* for(;;) */
if (GI2C1_UnselectSlave()!=ERR_OK) {
return ERR_FAILED;
}
return res;
}

Labels (1)
4 Replies

1,570 Views
BlackNight
NXP Employee
NXP Employee

Hi Gordon,

you can use

/*
** ===================================================================
**     Method      :  GI2C1_ReadBlockGeneric (component GenericI2C)
**     Description :
**         Read from the device a block with using additional control
**         and flags.
**     Parameters  :
**         NAME            - DESCRIPTION
**       * data            - Read buffer
**         dataSize        - Size of read buffer
**         flagsSend       - flags for the send transaction
**         flagsStart      - Start flags
**         flagsAck        - Acknowledge flags
**     Returns     :
**         ---             - Error code
** ===================================================================
*/
uint8_t GI2C1_ReadBlockGeneric(void* data, uint16_t dataSize, GI2C1_EnumSendFlags flags, GI2C1_EnumStartFlags flagsStart, GI2C1_EnumAckFlags flagsAck);

Which supports flags for sending. But currently this is only supported for software (bit banging I2C), not for the I2C_LDD.

If you would like to provide a contribution, I'm more than happy to include this into the driver.

Thanks,

Erich

1,570 Views
gordongao
Contributor II

I am use component to operate the I2C device.but is read one register all send a stop bit ,

0 Kudos
Reply

1,570 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi gordon,

   Please tell me what the chip you are using? Give me the part number.

   Now, take KL25 as an example, the stop code in KSDK is:

status_t I2C_MasterStop(I2C_Type *base)
{
    status_t result = kStatus_Success;
    uint16_t timeout = UINT16_MAX;

    /* Issue the STOP command on the bus. */
    base->C1 &= ~(I2C_C1_MST_MASK | I2C_C1_TX_MASK | I2C_C1_TXAK_MASK);

    /* Wait until data transfer complete. */
    while ((base->S & kI2C_BusBusyFlag) && (--timeout))
    {
    }

    if (timeout == 0)
    {
        result = kStatus_I2C_Timeout;
    }

    return result;
}

Actually, you can check our SDK code, which can be download from this link:

Welcome | MCUXpresso SDK Builder 

  


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,570 Views
gordongao
Contributor II

Thank you very much!, I am newer.

I use KL25demoboard.use component "InternalI2C",It create code mask the  "LDD_I2C_NO_SEND_STOP" in receive function.

My project use KL02. I could read different registers and don't send stop bit.When read over then send on stop bit?

0 Kudos
Reply