I want to program an external MCU MKL03Z32VFK4 using NXP FRDM-KL03Z board. How to do that?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to program an external MCU MKL03Z32VFK4 using NXP FRDM-KL03Z board. How to do that?

1,283 Views
nsmurthy
NXP Employee
NXP Employee

I have used our NXP Board - FRDM-KL03Z  for prototyping  a product. 

Now I wish to make a product out of the MCU  MKL03Z32VFK4 without using the freedom board.

 

Is there any way to flash program  an external MCU MKL03Z32VFK4 (part of a prototype board)  using Freedom board???

 

Waiting for a reply.

 

Thanks

-ns murthy

0 Kudos
Reply
1 Reply

1,167 Views
BlackNight
NXP Employee
NXP Employee

There are multiple ways/boards, but the process is very similar. A few links:

Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse 

Debug External Processors with USBDM and Freedom Board | MCU on Eclipse 

Using FRDM-K64F Board to debug another Kinetis Board | MCU on Eclipse 

Same thing applies for the FRDM-KL03Z, just check the schematics, cut a trace and solder a connector.

A better way is to use the LPC-Link2 with MCUXpresso IDE, which only costs $20, see Using the LPCXpresso V2/V3 Boards to Debug an external Board | MCU on Eclipse 

I hope this helps,

Erich

0 Kudos
Reply