I want to know can I use 16 bit ADC channels as single ended input in Kinetis K22.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to know can I use 16 bit ADC channels as single ended input in Kinetis K22.

1,301 Views
pushpraj
Contributor I
 
0 Kudos
Reply
1 Reply

1,296 Views
myke_predko
Senior Contributor III

Hi @pushpraj 

Yes you can.  Look at the "ADC# Channel Assignment for..." table in the Reference Manual of the device you are going to use.  

It will have the channel number for the ADC#_DP# pin (the positive input pin of the differential channel) and note you have to set the DIFF bit to zero.  

I highly recommend that you tie the DN# input to ground when you're using the DP# pin as a single channel.  

myke

0 Kudos
Reply