I want to Know how to use the K61 DDR controller and the Hard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to Know how to use the K61 DDR controller and the Hard

Jump to solution
2,106 Views
yongjunli
Contributor II

我想用k61的DDR控制器来配置一个大的内存,但是手册缺乏该介绍,硬件也不知道什么连接,我想获得一些指导

0 Kudos
Reply
1 Solution
1,877 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer can refer TWR-K70F120M board about hardware design how to connect K61 with DDR2 SDRAM device.

The TWR-K70F120 board hardware design resource package (includes schematics, layout, BOM info) could be downloaded from below link:

http://cache.freescale.com/files/soft_dev_tools/hardware_tools/printed_circuit_boards/bom/TWR-K70F12...

Kinetis K70 120 MHz Tower System Module|Freescale

Freescale also provides Kinetis DDR controller initialization tool could be downloaded from below link:

KINETIS_K70_DDR_INIT (Kinetis K70 DDR memory initialization tool):

http://cache.freescale.com/files/32bit/software_tools/initialization/boot_code_generation/KINETIS_K7...


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,878 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer can refer TWR-K70F120M board about hardware design how to connect K61 with DDR2 SDRAM device.

The TWR-K70F120 board hardware design resource package (includes schematics, layout, BOM info) could be downloaded from below link:

http://cache.freescale.com/files/soft_dev_tools/hardware_tools/printed_circuit_boards/bom/TWR-K70F12...

Kinetis K70 120 MHz Tower System Module|Freescale

Freescale also provides Kinetis DDR controller initialization tool could be downloaded from below link:

KINETIS_K70_DDR_INIT (Kinetis K70 DDR memory initialization tool):

http://cache.freescale.com/files/32bit/software_tools/initialization/boot_code_generation/KINETIS_K7...


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,877 Views
healy
NXP Employee
NXP Employee

Hi Hui

do we have a reference manual for "KINETIS_K70_DDR_INIT "?

I want to demonstrate it, but don't know why to use it.

thanks!

0 Kudos
Reply
1,877 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer <readMe.txt> embedded in KINETIS_K70_DDR_INIT (Kinetis K70 DDR memory initialization tool).

Wish it helps.

best regards,

Mike

0 Kudos
Reply
1,877 Views
yongjunli
Contributor II

thank you very match!this is my want ,thank you!

0 Kudos
Reply