I need a Serial Bootloader for the Kinetis K70. IAR is preferred, but I'll take CW or Keil if that is what you have. Thanks!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need a Serial Bootloader for the Kinetis K70. IAR is preferred, but I'll take CW or Keil if that is what you have. Thanks!

1,688 Views
johnatkins
Contributor I

The display board contains the K70 and Touchscreen. It is controlled by another board with another processor which manages the USB ports. We need to update our own firmware by plugging in a USB stick and having this control board send the appropriate s-records to the K70 on the display board, and reflash itself. This is a field firmware upgrade, so we can't use a J-Link or similar flashing device.

Labels (1)
0 Kudos
Reply
2 Replies

1,544 Views
mjbcswitzerland
Specialist V

Hi John

Serial loaders (USB-HOST [MSD - memory stick],  USB device (VCOM, MSD, Kboot), Modbus serial and TCP, Ethernet web server, I2C slave, SD-card, UART [srec, iHex, Kboot, AN2295]) with or without encryption.
Serial Loader: http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.pdf

for K70
http://www.utasker.com/kinetis/TWR-K70F120M.html

Turn-key (industrially proven over several years) solution projects for IAR, Keil, KDS, MCUXpresso, CodeWarrior, Atollic, Rowley Crossworks, CooCox, Green Hills, GCC, Visual Studio and complete K70 / memory stick / UART (approx. real-time) emulation in VisualStudio for testing, debugging, code reviews, efficient development modifications.

Free Open Source on GitHub (search uTasker) or supported version for professionals (request at links).

Regards

Mark

0 Kudos
Reply

1,544 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello John,

Please refer the following community post: 

https://community.nxp.com/docs/DOC-102616 

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply