TWR-K70 MSD HOST Bootloader based on AN4368 source code

Document created by Adrian Cano Employee on Oct 21, 2014Last modified by ebiz_ws_prod on Dec 13, 2017
Version 3Show Document
  • View in full screen mode

Hi Community members!

 

Here you can find the source code of the MSD Host Bootloader implemented on the AN4368 document using the TWR-K70F120M and CodeWarrior 10.6 and a document that describes the migration process of the original source code for the TWR-K60N512 to a TWR-K70F120M and the steps to use the application.

 

Attached you will find a image.s19 file created to be used with the bootloader application as an example.

 

This document and code are intended to demonstrate the use of the AN4368 source code on a 120 MHz device and CodeWarrior 10.6 but is not replacing the work done on the application note.

 

 

I hope this can be helpful for you!

 

Best Regards,

Adrian

 

 

If it was useful for you do not forget to click on the Like button. It would be nice!

Original Attachment has been moved to: TWR-K70-msd_bootloader.zip

2 people found this helpful

Attachments

Outcomes