I'm trying to communicate at 2.5Mbps using uart1 on mk10d.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I'm trying to communicate at 2.5Mbps using uart1 on mk10d.

924 次查看
tj_P
Contributor I

I want to use uart1 and dma to communicate rs485 at a transmission rate of 2.5mbps.

 

 

After the data is sent, it takes approximately 30 us seconds for the response to start in slave.

At this time, the first byte fills up with 0x00 intermittently, so can you suggest a solution for this?

0 项奖励
回复
1 回复

878 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @tj_P 

Can you tell me the clock speed of you MK10? 120MHz, 100MHz, 75MHz or 50MHz.

Can you provide me more details please? What do you mean with " for the response to start in slave"? UART does not uses master/slave modes.

Best Regards, Miguel.

0 项奖励
回复