I have writed a application with a serial bootloader support for TWR-K60D100M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have writed a application with a serial bootloader support for TWR-K60D100M

ソリューションへジャンプ
2,775件の閲覧回数
brandonk
Contributor II

  I have been trying to develop a serial bootloader based on AN2295 for TWR-K60D100M.

  Implemented the following ;

  1. Serial bootloader is good working.

  2. I used win_hc08sprg.exe tool on my PC.

K60 Serial Bootloader using tool.png

  3. I successed to download and erase, program my gpio application modified .lcf file to TWR-K60 board

      I refered to AN2295 pdf file, and modified .lcf file in my gpio application project.

      This my gpio application is good working in non bootloader environment(this means not modified .lcf file)

  4. But the application with the modified .lcf file is not working.

     /* This is original MEMORY SECTION
     MEMORY {
          m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x000001E0
          m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0007
FBF0
          m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000
          m_data_20000000 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00010000
          m_cfmprotrom (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
     }
     */

    // This is modified according to AN2295 document
     MEMORY {

          m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x000001E0
          m_text (RX) : ORIGIN = 0x00004410, LENGTH = 0x0007FFFF-0x00004410
          m_data (RW) : ORIGIN = 0x1FFF0000, LENGTH = 0x00010000
          m_data_20000000 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00010000
          m_cfmprotrom (RX) : ORIGIN = 0x00004400, LENGTH = 0x00000010
     }

  5. I followed the AN2295 document to load my application on the serial bootloader.

Please advise me to success writing an application with serial bootloader support.

1 解決策
2,075件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Your App linker file should be like below. I have used only with MQX App, but bare metal App is similar:

   

MEMORY {

serial_bootloader (RX) : ORIGIN=0x00000000, LENGHT = 0x00004000

m_interrupts (RX) : ORIGIN = 0x00004000, LENGTH = 0x00000410

m_text (RX) : ORIGIN = 0x00004420, LENGTH =  0x0007FFFF-0x00004420

m_data (RW) : ORIGIN = 0x1FFF0400, LENGTH = 0x0001FC00

m_data_20000000 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00010000

}

You don't need the cfmprotrom again, is defined in the bootloader. Remove that section.

And reserve 0x400 for the RAM vectors.

And your application needs to reallocate the vectors to RAM before procesing interrupts.

// Copy Application Stored Interrupt Vector table to RAM

pdst=(uint_32*)0x1FFF0000;

psrc=(uint_32*)0x4000;

for (i=0;i<0x100;i++,pdst++,psrc++)

{

*pdst=*psrc;

}

Then redirect the vector table to RAM by changing the SCB_VTOR like this:

 

// Redirect the vector table to the new copy in RAM

SCB_VTOR = (uint_32)0x1FFF0000;

Best Regards,

Luis


元の投稿で解決策を見る

1 返信
2,076件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Your App linker file should be like below. I have used only with MQX App, but bare metal App is similar:

   

MEMORY {

serial_bootloader (RX) : ORIGIN=0x00000000, LENGHT = 0x00004000

m_interrupts (RX) : ORIGIN = 0x00004000, LENGTH = 0x00000410

m_text (RX) : ORIGIN = 0x00004420, LENGTH =  0x0007FFFF-0x00004420

m_data (RW) : ORIGIN = 0x1FFF0400, LENGTH = 0x0001FC00

m_data_20000000 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00010000

}

You don't need the cfmprotrom again, is defined in the bootloader. Remove that section.

And reserve 0x400 for the RAM vectors.

And your application needs to reallocate the vectors to RAM before procesing interrupts.

// Copy Application Stored Interrupt Vector table to RAM

pdst=(uint_32*)0x1FFF0000;

psrc=(uint_32*)0x4000;

for (i=0;i<0x100;i++,pdst++,psrc++)

{

*pdst=*psrc;

}

Then redirect the vector table to RAM by changing the SCB_VTOR like this:

 

// Redirect the vector table to the new copy in RAM

SCB_VTOR = (uint_32)0x1FFF0000;

Best Regards,

Luis