I cannot find JLink Port in KDS PEMicro Debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I cannot find JLink Port in KDS PEMicro Debugger

1,548 Views
gloria
Contributor III

I follow the instruction and JLink CDC UART Port can be seen in device manager. However, I cannot find it in KDS PEMicro Debugger. Could you kindly help me about this?

One more question: I am using KDSK example -- gpio-example-frdmk64f. Why both 'debug' one and 'release' one are included in every type of debbugers? What are the differences between 'debug' and 'release'?

Thanks in advance!

pastedImage_0.png

pastedImage_1.png

Labels (1)
0 Kudos
Reply
3 Replies

1,372 Views
ivadorazinova
NXP Employee
NXP Employee

Dear Qingyuan Meng,

please, if you use J-Link, set please DBG SEGGER J-Link Debugging not PEMicro.

GDB.png

I hope it helps you,

Iva

0 Kudos
Reply

1,372 Views
gloria
Contributor III

Thanks Iva. If I want to use PEMicro, what change could I do? I use the frdm-k64f board. are these three buggers all avaliable for this board? Many thanks!

0 Kudos
Reply

1,372 Views
ivadorazinova
NXP Employee
NXP Employee

Hello ,

sure - if you want to use PEMicro, you should install OpenSDA from websites P&E Microcomputer Systems

and load new firmware.

Please, don ´t forget to following steps for loading :

1.Unplug the USB cable (if attached)

2.Press and hold the Reset button.

3. Plug in a USB cable from a USB Host to the OpenSDA USB port.

4. Release the RESET/Bootloader button.

5. A removable drive will be visible in the host file system with a volume label of BOOTLOADER

For more details you can visit OpenSDA User´s Guide​ or very useful could be also

Installation of OpenSDA Firmware on Freedom Board

Video Link : 3282

I hope it helps,

Iva

0 Kudos
Reply