I USED MK20DX128VLH5 FREEDOM BOARD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I USED MK20DX128VLH5 FREEDOM BOARD

1,196件の閲覧回数
dhanalakshmisre
Contributor I

I USED MK20DX128VLH5 FREEDOM BOARD

IN THAT HOW TO USE 6_bit DAC,SEND SAMPLE CODE...

ラベル(1)
0 件の賞賛
返信
1 返信

1,141件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

I'd highly recommend that you can refer to the 32.11 Digital-to-analog converter block diagram section for details.

The section illustrates the steps of using the 6-bit DAC

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信