I USED MK20DX128VLH5 FREEDOM BOARD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I USED MK20DX128VLH5 FREEDOM BOARD

1,203 Views
dhanalakshmisre
Contributor I

I USED MK20DX128VLH5 FREEDOM BOARD

IN THAT HOW TO USE 6_bit DAC,SEND SAMPLE CODE...

Labels (1)
0 Kudos
Reply
1 Reply

1,148 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,

I'd highly recommend that you can refer to the 32.11 Digital-to-analog converter block diagram section for details.

The section illustrates the steps of using the 6-bit DAC

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply