Hypothetically speaking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hypothetically speaking

1,854 Views
randyseedle
Contributor III

Hypothetically speaking, if you wanted to use a FRDM-K64 on a outer space flight what components would be most likely to fail in the environment of space ? Are there space rugedized components from NXP which could be used to replace the onboard components ? What about the PCB board itself. How would space affect the PCB ?

Randy

Labels (1)
2 Replies

1,740 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Randy,

 

Unfortunately, we do not have any aerospace compliant MCU, the nearest one on the K-Series devices is KEA automotive MCUs. Please check link below.

 

Arm Cortex-M0+|Kinetis KEA 32-bit Automotive MCUs | NXP 

 

In addition, I recommend you to read the following article about our Power Architecture Processors that are compliant with DO-254.

 

https://www.curtisswrightds.com/infocenter/white-papers/is-arm-for-airborne-platforms-in-military-an... 

 

Best regards,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,740 Views
bobpaddock
Senior Contributor III

Something at Micro Semi's Space page might lead you in a direction:

Applications - Space | Microsemi 

While very dated still has some interesting things to say:

Dialectrics for Space Vehicles:

https://apps.dtic.mil/dtic/tr/fulltext/u2/276867.pdf 

0 Kudos
Reply