How to view VECTPC on Kinetis MKL17Z256VLH4?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to view VECTPC on Kinetis MKL17Z256VLH4?

1,074 次查看
pcpro178
Contributor III

I'm trying to debug a hard fault on a MKL17Z256VLH4, and I'm not able to see VECTPC in the register view in Kinetis.  I've implemented the code in this app note in hopes of drilling down to where my hard fault is getting triggered.

Can anyone confirm if these register addresses (taken from the app note) are going to be correct for the ARM Cortex-M0+?

// Configurable Fault Status Register

// Consists of MMSR, BFSR and UFSR

_CFSR = (*((volatile unsigned long *)(0xE000ED28))) ;

// Hard Fault Status Register

_HFSR = (*((volatile unsigned long *)(0xE000ED2C))) ;

// Debug Fault Status Register

_DFSR = (*((volatile unsigned long *)(0xE000ED30))) ;

// Auxiliary Fault Status Register

_AFSR = (*((volatile unsigned long *)(0xE000ED3C))) ;

// Read the Fault Address Registers. These may not contain valid values.

// Check BFARVALID/MMARVALID to see if they are valid values

// MemManage Fault Address Register

_MMAR = (*((volatile unsigned long *)(0xE000ED34))) ;

// Bus Fault Address Register

_BFAR = (*((volatile unsigned long *)(0xE000ED38))) ;

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

913 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I would recommend our expert Derek's document << "Tracking down Hard Faults" >> about Kinetis product hard fault diagnostic.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复