How to use the TWR-LCD with Codewarrior 10.6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use the TWR-LCD with Codewarrior 10.6?

1,229件の閲覧回数
tudor-andreivra
Contributor I

Hi,

 

I am trying to use the TWR-LCD with or without TWRK60F120M.

I tried these examples mcuoneclipse/Examples/TWR-LCD at master · ErichStyger/mcuoneclipse · GitHub  . I followed the guide and updated Processor Experts components (at first it didn't recognize the CPU), then I installed Coldfire for CW (I think some components needed it) and I still have errors.

I have several errors.

47429_47429.PNGs1.PNG

47430_47430.PNGs2.PNG

 

Can somebody try these project and confirm that they work? There is a guide in the JM128 Bootloader project folder, and I attached the PE Update file (from the TWR LCD CD).

Thank you!

Original Attachment has been moved to: TWR-LCD_Components.PEupd.zip

タグ(1)
0 件の賞賛
返信
1 返信

1,135件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Tudor-Andrei Vrabie:

In your components view there are some missing components (the ones in gray). This implies you have not installed those and some files will not be generated.

Moreover the FAT and SD Card components have an error mark, then something must be configured incorrectly. Open the components properties and try to find the offending configurations.

Regards!

Jorge Gonzalez

0 件の賞賛
返信