How to use the K64 pit to design the delay function?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the K64 pit to design the delay function?

3,292 Views
zhailing
Contributor II

Hi

    I want to design a precise delay time;

for example:the stm32;

1.config the register  directly

void delay_ms(uint16_t ms) {  TIM6->PSC=35999;  TIM6->ARR=ms*2;  TIM6->CR1|=(1<<3);  TIM6->CR1|=0x1;  while((TIM6->SR&0X1)==0);  TIM6->SR=0; }


2.config the sdk
void TIM6_Delay_ms(uint16_t ms) {  /* 定义一个定时器基本定时初始化结构体变量 */  TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStruct;    /* 时钟预分频数为36000,在主频72M时,计数器每500us加1*/  TIM_TimeBaseInitStruct.TIM_Prescaler= 35999;    /* 自动重装载寄存器值 */  TIM_TimeBaseInitStruct.TIM_Period=ms*2;    /* 把上面的值配置到寄存器 */  TIM_TimeBaseInit(TIM6, &TIM_TimeBaseInitStruct);    /* 设置定时时间到了以后停止定时器计数 */  TIM_SelectOnePulseMode(TIM6, TIM_OPMode_Single);    /* 清除SR中的UIF标志 */  TIM_ClearFlag(TIM6, TIM_IT_Update);    /* 打开定时器6 */  TIM_Cmd(TIM6, ENABLE);    /* 检测定时时间是否到来 */  while(TIM_GetFlagStatus(TIM6, TIM_IT_Update)==RESET);   /* 软件清除更新标志 */  TIM_ClearFlag(TIM6, TIM_IT_Update); }

How to config the register of k64?

Thangks and best regards 

zhai

0 Kudos
Reply
3 Replies

3,086 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Zhai ling,

   About the K64 pit usage, please refer to our K64 sample code, which can be download from this link:

Welcome to Kinetis Expert | Kinetis Expert

 Click build an SDK, then select the board as FRDM-K64F120M, generate the code and download it, you can find the PIT code in folder:

SDK_2.0_FRDM-K64F\boards\frdmk64f\driver_examples\pit

pastedImage_1.png

The code in red frame can realize 1S PIT delay.

 

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,086 Views
zhailing
Contributor II

Hi Kerry

   I have solute the qustion!

Thanks very much!

zhai

0 Kudos
Reply

3,086 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Zhai ling,

   If your question is solved, please help to mark the correct answer to close this question.

   Thank you and have a nice day!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------