How to use i2c on the FRDM-KE02Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use i2c on the FRDM-KE02Z

846件の閲覧回数
danbean
Contributor I

I am doing a project with the FRDM-KE02Z board. I need to use i2c, which I am new to. The SDA and SCL pins are being used by an accelerometer  which i have no plan to use. How do I gain access to the pins without using the accelerometer? I know that you can use many devices on on i2c "line", other than that I am very new to this communication type. Any information would be extremely useful.

Dan Bean

Intern

タグ(1)
0 件の賞賛
返信
1 返信

678件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dan,

""

Please refer to here :Re: How to access PTA2 and PTA3 pins for I2C communication on FRDM-KE02Z board?

You are the same problem.

If still have any question , please contact us!


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信