How to use i2c on the FRDM-KE02Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use i2c on the FRDM-KE02Z

879 次查看
danbean
Contributor I

I am doing a project with the FRDM-KE02Z board. I need to use i2c, which I am new to. The SDA and SCL pins are being used by an accelerometer  which i have no plan to use. How do I gain access to the pins without using the accelerometer? I know that you can use many devices on on i2c "line", other than that I am very new to this communication type. Any information would be extremely useful.

Dan Bean

Intern

标记 (1)
0 项奖励
回复
1 回复

711 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dan,

""

Please refer to here :Re: How to access PTA2 and PTA3 pins for I2C communication on FRDM-KE02Z board?

You are the same problem.

If still have any question , please contact us!


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复