How to use external J-Link Plus with TWRK64F?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use external J-Link Plus with TWRK64F?

ソリューションへジャンプ
2,021件の閲覧回数
matthias2
Contributor I

I've plugged in the J-Link ARM Cortex-M cable into J5 - K64 JTAG, but the JLink's LED stays Orange, which indicates RESET is asserted, and it cannot access it.

The Getting Started Guide does not indicate any additional steps to configure the board for this.

How can I use an external JTAG with the TWRK64F?

(I've used the J-Link OpenSDA for a while which worked fine, but now it seems to got 'locked' while I was playing with blinky example and I figured I'd try the unlock with the real J-Link).

Thanks!

  Matthias

ラベル(1)
0 件の賞賛
返信
1 解決策
1,937件の閲覧回数
BlackNight
NXP Employee
NXP Employee
2 返答(返信)
1,937件の閲覧回数
matthias2
Contributor I

Thank for this simple answer. For others that end up here as well, here's the crucial information from the referenced blog post:

"Note that using the JTAG debug port (e.g. with Segger GDB server), the jumper J39 *has to be removed*! If the jumper is on, then the Segger GDB server silently quits (crashes?). Actually it shows an error message, then closes."

So, for external JTAG, remove J39.

I've went through the list of jumpers, but missed that one.

It would be helpful, if Jumper J39 could be mentioned in the TWR-K64F120M Tower Module User’s Guide, e.g. at 6.8.

0 件の賞賛
返信
1,938件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Matthias,

see First Steps with the Freescale TWR-K64F120M | MCU on Eclipse 

I hope this helps,

Erich