Hi,
For the UART is over sampling and in general it will using a frequency 16 times of the baud rate as over sampling frequency.
For example, if UART baud rate is 115200, customer need provide a 1.8432MHz (115200 X 16 ) square wave as the noise source.
During the UART communication, customer can connect 1.8432MHz square wave signal to UART RX pin.
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------