How to use GNU GSL library for LPCxpresso 4367

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use GNU GSL library for LPCxpresso 4367

1,417 次查看
shreyas123
Contributor III

Hi.

I need to use the GSL library in my program. I tried to follow the library linking procedure for LPC xpresso but the MCU linker is giving me these errors:


MCUXpressoIDE_10.3.0_2200\workspace\test1\Debug/../src/test1.c:53: undefined reference to `gsl_linalg_LU_decomp'
MCUXpressoIDE_10.3.0_2200\workspace\test1\Debug/../src/test1.c:56: undefined reference to `gsl_matrix_alloc'
MCUXpressoIDE_10.3.0_2200\workspace\test1\Debug/../src/test1.c:57: undefined reference to `gsl_linalg_LU_invert'

and so on for other functions as well.

Can someone please help me on this?

I have the libgsl.a and libgslcblas.a precompiled libraries for windows which works perfectly on codeblocks on windows with GCC compiler.

Do I have to cross compile the library again for Arm compiler? If yes, can you please provide me the procedure as well?

Thanks

标记 (2)
0 项奖励
回复
2 回复数

1,292 次查看
BlackNight
NXP Employee
NXP Employee

To anwer the easy question:

>>Do I have to cross compile the library again for Arm compiler?

Because your LPC device won't be able to run x86 code (or variants of it), you have to crosscomple il.

Erich

0 项奖励
回复

1,292 次查看
shreyas123
Contributor III

Thanks Erich. But can you please also tell me the procedure since this is my first time to cross compile something.

0 项奖励
回复