How to use GNU GSL library for LPCxpresso 4367

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use GNU GSL library for LPCxpresso 4367

1,413 Views
shreyas123
Contributor III

Hi.

I need to use the GSL library in my program. I tried to follow the library linking procedure for LPC xpresso but the MCU linker is giving me these errors:


MCUXpressoIDE_10.3.0_2200\workspace\test1\Debug/../src/test1.c:53: undefined reference to `gsl_linalg_LU_decomp'
MCUXpressoIDE_10.3.0_2200\workspace\test1\Debug/../src/test1.c:56: undefined reference to `gsl_matrix_alloc'
MCUXpressoIDE_10.3.0_2200\workspace\test1\Debug/../src/test1.c:57: undefined reference to `gsl_linalg_LU_invert'

and so on for other functions as well.

Can someone please help me on this?

I have the libgsl.a and libgslcblas.a precompiled libraries for windows which works perfectly on codeblocks on windows with GCC compiler.

Do I have to cross compile the library again for Arm compiler? If yes, can you please provide me the procedure as well?

Thanks

0 Kudos
Reply
2 Replies

1,288 Views
BlackNight
NXP Employee
NXP Employee

To anwer the easy question:

>>Do I have to cross compile the library again for Arm compiler?

Because your LPC device won't be able to run x86 code (or variants of it), you have to crosscomple il.

Erich

0 Kudos
Reply

1,288 Views
shreyas123
Contributor III

Thanks Erich. But can you please also tell me the procedure since this is my first time to cross compile something.

0 Kudos
Reply