How to use DMA, for wave file data transfer to interface AUDIO SGTL CODEC with K70

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use DMA, for wave file data transfer to interface AUDIO SGTL CODEC with K70

1,401 次查看
deepakbhagat
Contributor II

I was able to communicated with with AUDIO SGTL CODEC with K70 through i2s. It was found that there is considerable use of cpu while playing the audio wave file so can I get help on how i can use DMA to optimize the use of cpu time.

标签 (1)
0 项奖励
回复
1 回复

1,139 次查看
egoodii
Senior Contributor III

I don't know what variant (Rev 1.x or Rev 2.x) I2S you are dealing with, but I suspect their DMA operations are at least 'very similar'.  You will find my Rev 1.x setup here:

https://community.freescale.com/message/82190#82190

That is particularly set up to interleave/de-interleave six 16-bit audio channels from consecutive linear ping-pong buffers to their respective CoDecs thru I2S network mode.  I believe the 'defines' there allow for reasonable customization (except whatever I missed!).  The DMA minor-loop/major-loop format, with sophisticated counter-manipulation capabilities at each level, in conjunction with 'half loop' interrupts, allows this unattended data handling.