How to unlock K64F on TWRK64F120M?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to unlock K64F on TWRK64F120M?

1,021 次查看
matthias2
Contributor I

Hi. Without playing with security, the K64F got into a read protected mode. That's from JLink tool with J-Link OpenSDA

Connecting to target via SWD
InitTarget()
Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set.
For debugger connection the device needs to be unsecured.
Note: Unsecuring will trigger a mass erase of the internal flash.
Device will be unsecured now.
Timeout while unsecuring device. Erase never starts.

NXP Web Chat suggested to try P&E Recovery Tool. However, after putting PE firmware on the OpenSDA, the recovery tool couldn't find the board.

I'd also like to try with my J-Link Plus, but I couldn't figure out what configuration is needed to use it asides from pluggin the ARM Cortex M connector into the K64 JTAG header J5.

Any other ideas?

标签 (1)
0 项奖励
回复
1 回复

885 次查看
matthias2
Contributor I

Thanks to this answer How to use external J-Link Plus with TWRK64F?, I was able to connect a J-Link Plus externally. Then, I've used the GUI Flash tool in MCUXpresso with the J-Link, and selected the "Resurrect locked Kinetis device", which worked the first time.

So, in my setup, I was (only) able to unlock it using an external J-Link Plus.

0 项奖励
回复