How to set the PHY address for LAN8720A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set the PHY address for LAN8720A

6,889 次查看
chaitannyamahat
Contributor II

Hi ,

I am programming a custom board based on MK60DN512 chip.

We are using LAN8720A as a PHY device. Tricky part is determing /setting the PHY ID.

I don't know what is the default ID. In the datasheet they have mentioned that the we have to assert RXER pin low to set the PHY ID. How to assert RXER pin low when it is not configure as GPIO.

I have written a simple code which tries to read the PHY_PHYIDR1 register of LAN8720. I am not getting any valid data.

do

  {

    vTaskDelay( netifLINK_DELAY );

    usData = 0xffff;

    ret=mii_read( 0, id, PHY_PHYIDR1, &usData );

    id++;   

  } while( usData == 0xffff);

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

4,262 次查看
mjbcswitzerland
Specialist V

Hi

The PHY address depends on the PULL-UP / PULL-DOWN resistors on its STRAP inputs as the PHY exits reset.

If you read on all possible PHY addresses (which I think you are doing) but don't get an answer it is likely to be a HW problem. Do you have a pullup resistor on the MDIO line? Also you could check the clock rate that the interface is sending to ensure that it is not too fast (2.5MHz is typical max. speed).

Regards

Mark

4,262 次查看
trilokjt
Contributor III

Hi,

I have same issue,on MDC pin I'm getting around 4.5Mhz clock, Please tell how to sort out the Problem.

0 项奖励
回复

4,262 次查看
chaitannyamahat
Contributor II

Hello Mark,

Thanks for your valuable insight.

I have verified the straps , MDIO is OK.

I tried the same program on Tower board, works fine. I think the issue is with hardware, investigating that time being.