How to read bandgap?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,318件の閲覧回数
adampribyl
Contributor I

I am trying to do a temperature sensor measurement according AN3031 on FRDM-KL25. I used PE to generate the code. I can read stable results from ADC for tempsensor and for Vrefh but the internal bandgap is floating a lot. Even the +-3% accuracy of internal bandgap can not explain it.

The code is as "easy" as this:

      AD1_MeasureChan(1, 0);

      AD1_GetChanValue16(0, &adcvalue);

      printf("ADC value: %d, ", adcvalue);

      AD1_MeasureChan(1, 2);

      AD1_GetChanValue16(2, &adcvalue);

      printf("Bandgap: %d ", adcvalue);

      AD1_MeasureChan(1, 1);

      AD1_GetChanValue16(1, &adcvalue);

      printf("Temperature sensor: %d, ", adcvalue);

      AD1_MeasureChan(1, 2);

      AD1_GetChanValue16(2, &adcvalue);

      printf("Bandgap: %d ", adcvalue);

      AD1_MeasureChan(1, 3);

      AD1_GetChanValue16(3, &adcvalue);

      printf("Vrefh: %d \r\n", adcvalue);

ADC is in 16bit mode single ended 10us, low power mode, high speed conversion, async clock. With 1 conversion I receive completely insane values after bandgap read looks like it depends on the previous read, with 64 conversion it is from 20000-26000 which is way too much to do any reasonable calculation of the temperature. I can change the ADC properties but is has no influence on the results. I may be doing something completely wrong, but ATM do not see what.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,148件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Please check my attached project, which use FRDM-KL25Z board to read bandgap voltage with ADC0_A.

Please check PMC_REGSC [BGBE] bit need be set to enable Bandgap generate voltage.

Wish it helps.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,149件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Please check my attached project, which use FRDM-KL25Z board to read bandgap voltage with ADC0_A.

Please check PMC_REGSC [BGBE] bit need be set to enable Bandgap generate voltage.

Wish it helps.

0 件の賞賛
返信
3,148件の閲覧回数
adampribyl
Contributor I

Thanks a lot, it is in Ref. manual, I just missed this note "2".

0 件の賞賛
返信
3,147件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Adam,

I will try to do the same test with FRDM-KL25Z board. I will let you know when I got any info.

Thank you for the patience.

B.R.

Ma Hui

0 件の賞賛
返信