How to program k70 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to program k70 board

1,269件の閲覧回数
sameerarvikar
Contributor III

I am trying to program k70 cortex m4 controller

I don't have tower ,just the board

I don't have jtag programmer,just a usb cable that came with

So is it possible to program it with usb port 

And how to do it

タグ(1)
0 件の賞賛
返信
1 返信

1,176件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

If the board K70 chip with USB bootloader software already been programed, then customer can load image to K70 with USB port.

If the K70 chip is empty, there does need a JTAG programmer tool, such as Segger J-Link or P&E USB Multilink Universal.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信