How to power USB OTG in FRDM-K64F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to power USB OTG in FRDM-K64F

1,165 次查看
xavierx
Contributor I

Hi,

I'm trying to see if I can avoid soldering the FRDM-K64 board for this and I  need some further clarification from the documentation about the FRDM-K64F board. Without using the OpenSDA port, if my program uses the USB OTG port to interact with a device, is it enough to provide 5V through P5V_USB (Pin 10 of header J3) to power the board?

Thanks in advance,

Xavier

标签 (2)
0 项奖励
回复
1 回复

911 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Xavier,

Yes, I think so.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------