How to modify the program start address and vector table address in MCUXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to modify the program start address and vector table address in MCUXpresso

2,374 次查看
1054144848
Contributor II

I am developing an AN2295-based boot loader program. Now I need to modify the application's ROM start address and vector table address.In the AN2295 Developer's Serial Bootloader manual, IAR and CodeWarrior have linker files (ICF file in IAR and in LCF file in CodeWarrior) that can be modified. Then, where is the linker files of MCUXpresso, how to modify it?Memoryallocation.pngkl60.png

标记 (2)
0 项奖励
回复
1 回复

2,235 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello [email protected]

 

We have 2 ways to do that.

One way is directly at the project explorer, you need to go to the debug folder where the files are located:

 pastedImage_2.png

Other way to modify memory address is through MCU settings. You can access to this tab by going to your project properties:

pastedImage_1.png

 

For more information I suggest you to take a look under chapter 18 "Memory Configuration and Linker Scripts"

https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf

 

 

Let me know if this helps

Best regards

 

Omar

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 项奖励
回复