Hello Huaping,
you can simply concatenate two files in the following way as
% cat BOOT.hex APP.hex > ALL.hex
and delete S8 or S9 record.
% grep -v 'S[89]' ALL.hex > ALL2.hex
Then you can get it.
% arm-none-eabi-objdump -D -M force-thumb -m armv5te ALL2.hex
ALL2.hex: file format srec
Disassembly of section .sec1:
00000000 <.sec1>:
0: 3000 adds r0, #0
2: 2000 movs r0, #0
4: 09b1 lsrs r1, r6, #6
6: 0000 movs r0, r0
8: 0949 lsrs r1, r1, #5
a: 0000 movs r0, r0
c: 0949 lsrs r1, r1, #5
...
2a: 0000 movs r0, r0
2c: 0949 lsrs r1, r1, #5
...
--[snip]--
9b0: f005 fe38 bl 0x6624
9b4: f7ff ffce bl 0x954
9b8: f7ff ffe8 bl 0x98c
9bc: f005 fe0a bl 0x65d4
9c0: f005 fda6 bl 0x6510
9c4: f005 fe3c bl 0x6640
9c8: 4b04 ldr r3, [pc, #16] ; (0x9dc)
--[snip]--
6624: 4b05 ldr r3, [pc, #20] ; (0x663c)
6626: 1c18 adds r0, r3, #0
6628: 2800 cmp r0, #0
662a: d005 beq.n 0x6638
662c: 4685 mov sp, r0
662e: b081 sub sp, #4
6630: 2000 movs r0, #0
6632: 43c0 mvns r0, r0
6634: 9000 str r0, [sp, #0]
6636: b001 add sp, #4
6638: 46f7 mov pc, lr
663a: 4770 bx lr
--[snip]--
Disassembly of section .sec3:
00000400 <.sec3>:
400: ffff ffff ; <UNDEFINED> instruction: 0xffffffff
404: ffff ffff ; <UNDEFINED> instruction: 0xffffffff
408: ffff ffff ; <UNDEFINED> instruction: 0xffffffff
40c: ffff fffe ; <UNDEFINED> instruction: 0xfffffffe
Disassembly of section .sec4:
0000be00 <.sec4>:
be00: 0000 movs r0, r0
be02: 0cbe lsrs r6, r7, #18
be04: 0100 lsls r0, r0, #4
be06: ffff ffff ; <UNDEFINED> instruction: 0xffffffff
be0a: ffff a1a1 vaddw.u<illegal width 64> q13, <illegal reg q15.5>, d17
be0e: 1a1a subs r2, r3, r0
--[snip]--
% arm-none-eabi-objcopy -I srec -O binary ALL2.hex ALL2.bin
% od -t x2 -A x ALL2.bin
000000 3000 2000 09b1 0000 0949 0000 0949 0000
000010 0000 0000 0000 0000 0000 0000 0000 0000
000020 0000 0000 0000 0000 0000 0000 0949 0000
000030 0000 0000 0000 0000 0949 0000 0949 0000
000040 0949 0000 0949 0000 0949 0000 0949 0000
*
0000c0 0000 0000 0000 0000 0000 0000 0000 0000
*
000400 ffff ffff ffff ffff ffff ffff ffff fffe
000410 0000 0000 0000 0000 0000 0000 0000 0000
*
000800 0000 80c0 0100 ffff ffff ffff a1a1 1a1a
000810 ffff ffff ffff ffff ffff ffff ffff ffff
000820 ffff ffff ffff ffff 0000 0001 5300 4630
000830 ffff ffff ffff ffff ffff ffff ffff ffff
*
000880 b402 4671 0849 0049 5609 0049 448e bc02
000890 4770 46c0 b402 4671 0849 0049 5c09 0049
0008a0 448e bc02 4770 46c0 2900 d034 2301 2200
--[snip]--
Isn't it OK?
Best regards,
Yasuhiko Koumoto.