How to map ISR to a HW interrupt?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to map ISR to a HW interrupt?

Jump to solution
6,956 Views
willx
Contributor IV

Hi,

I just started development with FRDM-KL03 board and doing some SPI/I2C stuff. I would like to know how do I map an ISR that I write to service a certain HW interrupt.

It's a beginner question, but any help would be appreciated.

Thanks!

Labels (1)
Tags (4)
1 Solution
5,142 Views
willx
Contributor IV

I was able to just make use the default Kinetis_startup.s that includes the vector table mapping and it worked since I name my ISR SPI0_IRQHandler().

Thanks all for your help!

View solution in original post

7 Replies
5,143 Views
willx
Contributor IV

I was able to just make use the default Kinetis_startup.s that includes the vector table mapping and it worked since I name my ISR SPI0_IRQHandler().

Thanks all for your help!

5,142 Views
yasuhikokoumoto
Senior Contributor I

Hi Will X-san,

I don't understand correctly what is your intension. Do you make programs from the scratch? It would be a little difficult. I think you can re-use the FRDM-KL25Z Sample Code probably even for KL03. The Sample Code can get from the freescale site (http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL2x&fpsp=1&tab=Design_Tools_Tab).

Software Development Tools > Lab and Test Software > KL25_SC

If you use the KL25 Sample Code, you can map SPI/I2C ISRs for each interrupt to modify isr.h file in the sample code as follows.

----[snip]-----
void your_SPI_handler();
void your_I2C_handler();

#under   VECTOR_026
#define  VECTOR_026  your_SPI_handler

#under   VECTOR_024
#define  VECTOR_024  your_I2C_handler
----[snip]-----


I am not sure whether the vector number of KL25Z is the same as KL03. From the KL03 reference manual it seems to be the same.
Do this help you?

Best regards,
Yasuhiko Koumoto.

0 Kudos
Reply
5,142 Views
willx
Contributor IV

Thanks for your answer Yasuhiko-san!

Yes, I am making a program from scratch. I am not basing it on anything and I am enabling the HW interrupts for I2C and SPI but I don't know how to map a handler function to service those interrupts.

In the snippet you provided, where are VECTOR_024 and VECTOR_026 defined? They are defined anywhere in my project. I am using MKL03Z4.h file that contains all the chip related definitions.

0 Kudos
Reply
5,142 Views
gibbon1
Contributor III

If you download the code sample code Yasuhiko-san pointed you to, you'll see a file named startup_MKL25Z4.s


That file contains a table of interrupt vectors with handy names like SPI0_IRQHandler and I2C0_IRQHandler by default these have a weak link to Default_Handler. What that means is if you don't provide a function with that name in your code, than then Default_Handler() gets called if the interrupt occurs. However if you supply and interrupt handler by simply creating a function of that name, it gets linked instead of the default handler.


Note, I'm not really up on the freescale demo code. Some examples instead of the vector table being defined and an assemble (.s) file, it's defined in a .c file instead. But the effect is exactly the same.


So for an spi handler likely


void SPI0_IRQHandler(void)

{

    // your code here

}


This should totally work. Note an easy test is to use a pin change interrupt to toggle and LED.


Good luck, bare metal projects are often a bit painful to get off the ground.






5,142 Views
yasuhikokoumoto
Senior Contributor I

Hello  Matthew-san,

thank you for your explanations. they would be almost perfect. Also I would add some comments.
VECTOR_024 and VECTOR_026 are defined in the vector.h at
    ${PROJ_ROOT}\cpu\vector.h
which is contained in the KL25 Sample Code package.
The vector.h is included by the vector.c at the same directory.

-----[snip]-------
#if (defined(KEIL))
const vector_entry  __vector_table[] = //@ ".intvec" =
#elif (defined(IAR))
#pragma location = ".intvec"
const vector_entry  __vector_table[] = //@ ".intvec" =
#elif (defined(CW))
const vector_entry __attribute__ ((section(".vectortable"))) __vector_table[] = //@ ".intvec" =
#endif
{
   VECTOR_000,           /* Initial SP           */
   VECTOR_001,           /* Initial PC           */
   VECTOR_002,
   ...........
   VECTOR_PADDING,
   VECTOR_PADDING,
#ifndef CW
   CONFIG_1,
   CONFIG_2,
   CONFIG_3,
   CONFIG_4,
#endif

};
-----[snip]-------

And the above tabe is referred in the startup.c like as fllowing.

-----[snip]-------
#if (defined(KEIL))
extern uint32 Image$$VECTOR_ROM$$Base[];
extern uint32 Image$$VECTOR_RAM$$Base[];
#define __VECTOR_TABLE Image$$VECTOR_ROM$$Base 
#define __VECTOR_RAM Image$$VECTOR_RAM$$Base 
#elif (defined(IAR))
/* Addresses for VECTOR_TABLE and VECTOR_RAM come from the linker file */
extern uint32 __VECTOR_TABLE[];
extern uint32 __VECTOR_RAM[];
#elif (defined(CW))
        #define __VECTOR_TABLE __vector_table 
#define __VECTOR_RAM   __vector_ram
extern uint32 __VECTOR_TABLE[];
extern uint32 __VECTOR_RAM[];
#endif

    /* Copy the vector table to RAM */
    if (__VECTOR_RAM != __VECTOR_TABLE)
    {
        for (n = 0; n < 0x104; n++)
            __VECTOR_RAM[n] = __VECTOR_TABLE[n];
    }
    /* Point the VTOR to the new copy of the vector table */
    write_vtor((uint32)__VECTOR_RAM);   
-----[snip]-------

The startup.c is located at
    ${PROJ_ROOT}\common\startup.c.

I wonder why Will X-san don't use the sample code package because KL03 sample codes are re-used from KL25Z on the freescale site (http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KL02&fpsp=1&tab=Design_Tools_Tab).

Best regards,
Yasuhiko Koumoto.

5,142 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Will,

Freescale provides KSDK software for KL03 chip.

Please download [Freescale Kinetis SDK_1.0.0 for the FRDM-KL03Z - Windows installer] from below link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-KL03Z&fpsp=1&tab=Design_Tools_Ta...

After installation the KSDK for KL03Z software, customer could find example demo at default path:

C:\Freescale\KSDK_1.0.0-KL03Z\demos

Just using [rtc_func] as an example, the interrupt ISR list at <startup_MKL03Z4.s> file with vector table to related ISR function.

The ISR function should with the same name as <startup_MKL03Z4.s>, and customer could find RTC IRQ ISR and RTC second IRQ ISR function located <rtc_func.c> file line 74:

/* override the RTC IRQ handler */

void RTC_IRQHandler(void)

{

    if (RTC_DRV_IsAlarmPending(0))

    {

        gAlarmPending = 1;

        /* disable alarm interrupt */

        RTC_DRV_SetAlarmIntCmd(0, false);

    }

}

/* override the RTC Second IRQ handler */

void RTC_Seconds_IRQHandler(void)

{

    gSecsFlag = true;

}


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

5,142 Views
mjbcswitzerland
Specialist V
0 Kudos
Reply