How to keep USB alive while entering bootloader?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to keep USB alive while entering bootloader?

2,090件の閲覧回数
georgschmidt
Contributor III

Hi,

I'm working on a USB-Bootloader for my Kinetis K60 project.

I have to seperate projects (bootloader and application) stored in different Flash-sections.

Currently I'm able to jump from application to bootloader and back.

The problem is, that I loose the USB-connection (running on USB0-module) after jumping from one section to the other.

If I do a complete reinitialisation of the USB, the USB disconnects and reconnects imediately after the jump.

But I don't want the PC to recognize the jump, so I have to recover some settings of the USB-module.

But which?

I tried to recover the BDT-Table contents, but this seems not to be enough. Do I need to recover the Endpoint-Buffers also?

Has anyone done something like this without using a RTOS or Processor Expert?

Regards,

Georg

ラベル(1)
タグ(2)
2 返答(返信)

1,883件の閲覧回数
juanma_clautron
Contributor II

Hi Georg!

How do you jump from the app to the bootloader "Currently I'm able to jump from application to bootloader and back." ???

Thanks

0 件の賞賛
返信

1,883件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Georg:

I think the jump cannot be transparent for the PC. The bootloader and the application do not share the same BDT table, instead each one has its table, and the transition is detected, so as you mentioned you need to reinitialize the USB.


Regards!,
Jorge Gonzalez