How to interace K81 with i.MX6?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to interace K81 with i.MX6?

1,799 Views
shree97
Contributor I

I want to interface K81 with i.MX6 solo/dualite over SPI interface.

I want to know whether the driver for this is already available or not?

If I need to develop the driver in which register of K81 I should write/read the data?

Please guide me regarding this issue.

Thanks & Regards,

Shree

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,602 Views
miduo
NXP Employee
NXP Employee

Hi,

Yes, we do has the K81 QSPI driver ready. But I am not sure if it will work with I.MX6. Because I.MX use a different IDE(Linux or Android.)  You may make reference this thread for the IMX related:https://community.nxp.com/message/837810 

0 Kudos
Reply

1,602 Views
shree97
Contributor I

Hello Fang Li,

I referred that thread but its giving example of accessing the spi device from user space.

But I want  to develop the  SPI protocol driver by treating K81 as slave device.

Kindly guide me.

Thanks & Regards,

Shree 

0 Kudos
Reply