How to get disconnection event with reason 278 immediately

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get disconnection event with reason 278 immediately

1,522件の閲覧回数
FedericoWegher
Contributor III

Hello.

I am using NXP KW38 with SDK 2.6.9. In my application there is a central and a peripheral BLE devices.

When central forces disconnection, I would like to get the disconnection event (with reason 278) as soon as possible, not after supervision timeout, on both central and peripheral.

How can I achieve this?

タグ(2)
0 件の賞賛
返信
1 返信

1,503件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Federico, I hope you're doing well!

 

These functions are implemented in the pre-compiled section of the NXP BLE Stack. Error and status codes are implemented following the BLE Specification established by the Bluetooth SIG.

 

Still, could you please provide some more information about the intention with the modification you're planning? And also some more details about the disconnection reason you want to implement?

 

Best regards,

Sebastian

0 件の賞賛
返信