How to get FRDM-KL03Z to start in ROM bootloader?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get FRDM-KL03Z to start in ROM bootloader?

ソリューションへジャンプ
1,667件の閲覧回数
grantedwards
Contributor I

I've got an FRDM-KL03Z which I would like to start in ROM bootloader mode.

Unfortunately, it seems to have an application in FLASH (I don't know/care what the app is).

I'm using Linux as my development host.

The OpenSDA docs talk about a flash programmer app, but it only runs under MS-Windows,

Eval boards for other vendors/parts always have had jumper(s) that forced the part's boot mode, but this board doesn't seem to have anything like that.

How do I erase flash so that it will boot up in the ROM bootloader?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,497件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Grant,

You can use the following steps to force the MCU enter the ROM bootloader:

First of all, hold down the SW3 button, then reset the MCU and the MCU will enter the ROM bootloader.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,498件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Grant,

You can use the following steps to force the MCU enter the ROM bootloader:

First of all, hold down the SW3 button, then reset the MCU and the MCU will enter the ROM bootloader.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信