How to flush the program to MK64FN1M0VLL12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flush the program to MK64FN1M0VLL12

2,117件の閲覧回数
kazukiyamashita
Contributor II

Method of operation of the MK64FN1M0VLL12 question about.

I'd like make the following way, Do you have any URL such methods have been described?

1. to write operation program. (LED Blinky, etc.)

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,985件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi kazuki,

     If you want to program the MK64FN1M0VLL12,  you can use the debugger, eg:JLINK, P&E multilink, ect.

    And associate with the IDE to download the code to your chip.

    If you are using the official board tower or freedom, this board have the onboard debugger, you can download the code to the chip directly.

    If you use your own board, you can use the JLINK or Mulitlink to download the code.

    About the question, write operation program. (LED Blinky, etc.), you can refer to our sample code in KSDK2.0-FRDM-K64.

    Please download the sample code from this link:

Welcome to Kinetis Expert | Kinetis Expert 

   Click build an SDK, then choose board FRDM-K64.

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,985件の閲覧回数
kazukiyamashita
Contributor II

The problem is resolved. Thank you very much!

0 件の賞賛
返信

1,986件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Thank you for your information updated.

 If your problem is resolved, please help to mark it as answered.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信