Hello,
I'm using Codewarrior V10.4 build id:130425 with processor expert in a custom PCB based in K60 processor.
I'm able to build and debug my projects in RAM or FLASH options, and for debugging everything seems to work fine, but when I run the project (For testing purposes is just a blinking led) with the FLASH option, it did not really "flash" the code, because when I power off and on the device, it did no execute the code (The led did not blink).
I had been trying to flash the code with the "Flash Programmer" (the blue thunderbolt) but, despite it appears in the console that the code was succesfully downloaded, the device is still dead after power off and on.
I already try the steps in this blog :
http://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/
And I also followed these videos:
https://community.freescale.com/message/356842#356842
But I still have the same problem, when I turn on the power buton the LED do not blink
>:(
What I want is to flash the code in the processor to be executed forever and ever after power on
any idea???