How to enable UART3 on TWR-K60D100M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable UART3 on TWR-K60D100M

2,052件の閲覧回数
yarannan
Contributor III

I am trying to modify  a demo application on KDS 2.0 with KSDK 1.1.0. I only have twr-k60d110m and TWR-IND-IO. Am i being able to change

default setting to UART3? Does anyone know?

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,843件の閲覧回数
yarannan
Contributor III

So hey guys thanks for helping me. I still dont know how, but i will try it later.

0 件の賞賛
返信

1,843件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hi Yaran Nan,

I don't know which demo are you using.

let's take hello_world_twrk60d100m as an example.

To modify the debug console output to UART3, you need just modify BOARD_DEBUG_UART_INSTANCE from 5 to 3.

This Macro is defined in line 43 in board.h.

hope it helps!

0 件の賞賛
返信

1,843件の閲覧回数
mjbcswitzerland
Specialist V

Hi Yaran

I can't help with the demos but if you want full flexibility using KDS you can look at µTasker Kinetis TWR-K60D100M support

1. Choose the UART to be used as follows (example of opening the interface on any channel (0..5) and sending a "Hello, World!" output.

TTYTABLE tInterfaceParameters;

tInterfaceParameters.Channel = 3; // 0, 1, 2, 3 ,4 or 5

tInterfaceParameters.ucSpeed = SERIAL_BAUD_115200;

tInterfaceParameters.Config = (CHAR_8 + NO_PARITY + ONE_STOP + USE_XON_OFF + CHAR_MODE);

tInterfaceParameters.ucDMAConfig = UART_TX_DMA;

..

SerialPortID = fnOpen(TYPE_TTY, FOR_I_O, &tInterfaceParameters);

fnWrite(SerialPortID, "Hello, World!", 13);

2. Fine tune the UART's pin multiplexing by choosing from a set of defines:

//#define UART0_A_LOW                                          // alternative UART0 pin mapping
//#define UART0_ON_B                                           // alternative UART0 pin mapping
//#define UART0_ON_D                                           // alternative UART0 pin mapping
//#define UART1_ON_C                                           // alternative UART1 pin mapping
//#define UART2_ON_E                                           // alternative UART2 pin mapping
//#define UART2_ON_F                                           // alternative UART2 pin mapping
//#define UART3_ON_B                                           // alternative UART3 pin mapping
//#define UART3_ON_F                                           // alternative UART3 pin mapping
#define UART3_ON_C                                           // alternative UART3 pin mapping
//#define UART4_ON_C                                           // alternative UART4 pin mapping
//#define UART5_ON_D                                           // alternative UART5 pin mapping

Regards

Mark

Kinetis: µTasker Kinetis support

K60: µTasker Kinetis TWR-K60N512 support / µTasker Kinetis TWR-K60D100M support / µTasker Kinetis TWR-K60F120M support

UARTs: http://www.utasker.com/docs/uTasker/uTaskerUART.PDF

For the complete "out-of-the-box" Kinetis experience and faster time to market