How to download program to kl26 mcu by uart port ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to download program to kl26 mcu by uart port ?

1,269件の閲覧回数
junwang1
Contributor II

How to download program to kl26 mcu by uart port ?

0 件の賞賛
返信
2 返答(返信)

1,181件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

This is the same question as your another post:

HOW  

Please refer to that post, I already reply you in that post.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,181件の閲覧回数
mjbcswitzerland
Specialist V

Hi

See also
http://www.utasker.com/kinetis/FRDM-KL26Z.html
http://www.utasker.com/kinetis/TEENSY_LC.html

for serial loading using KBOOT, SREC, IHEX, AN2295 developer's loader and/or USB-MSD (device and/or host), SD card (or even Ethernet using external ENC424J600)....

Regards

Mark

Kinetis for professionals: http://www.utasker.com/kinetis.html

0 件の賞賛
返信